如题,我尝试把DSP2833x_CSMPasswords.asm加进工程中,修改密码,无果。希望能得到完整的步骤指导,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,我尝试把DSP2833x_CSMPasswords.asm加进工程中,修改密码,无果。希望能得到完整的步骤指导,谢谢。
我用28335试了,然后提示下次连接的时候就上锁了。
然后尝试连接,出现以下提示。
Error connecting to the target:
(Error -233 @ 0x0)
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
(Emulation package 5.1.507.0)
连接不上,有没有什么办法可以解决,谢谢。