Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG
Sorry, my issue was sent to the TI Customer Support Center but was not resolved. I am sending it again to the "C2000 Microcontroller Forum" to seek assistance. The problem is as follows:
After importing the example project in CCS 20.4.0, the device package cannot be selected.
TI Engineer,
Hello!
After importing the example project in CCS 20.4.0, when using the internal SysConfig 1.26 to configure the .sysconfig file, I am unable to select the device package. The list only allows selecting the 100PZ package, and there are no options for 80PN or 64PM. If I want to use an 80PN or 64PM package device, could you please advise on how to proceed?
Best regards.
Yong Liu