This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CLA调试问题求助



F28035,C28x程序load后,CLA symbols也load好,然后C28x run(F8)且C28x代码无断点,CLA程序开始运行——

1、为什么我看到的CLA程序在CCS中表象看起来PC指针(光标)是停下的,按F8时又提示warning说device running?

2、在C28x处于无断点run情况下,CLA中周期运行的程序如task1在CCSv5.5中会显示时不时刷新一下——PC指针一会儿停在这儿,一会儿停在那儿——这会导致一个表象上看起来很严重的问题:Graph观察Expression中的变量会出现“突变”数据,如果实际上数据的确在突变,那我的控制算法就肯定会出大问题。

这样会导致我无法连着仿真器进行debug——因为过程数据会因为CLA程序run过程中的不定期刷新导致“突变”。

请问,这该怎么破?急急急