This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: TMS320F2800137芯片VCU模块

Part Number: TMS320F2800137
Other Parts Discussed in Thread: C2000WARE

我们想要使用TI提供的CRC32的计算方式,对于下边这个函数,我们使用TMS320F2800039芯片可以使用这个函数的得到CRC32的校验值,但是使用TMS320F2800137芯片使用这个函数的时候,仿真的时候可以进入到函数内部执行,但是得到的CRC32的校验值是0,查找芯片手册,没有找到关于这个的相关资料,在网上查找资料说,使用这个函数芯片内部需要有VCU模块,网上说039的有VCU模块,137的芯片没有这个模块,所以想问你们137是否有这个模块,使用这个函数是否需要这个模块,如果不需要的话,想问一下使用这个函数的话,需要的头文件vcu2_crc.h和vcu2_types.h两个芯片是否通用,请帮忙解释一下,谢谢!

Uint32 GetCRC32(Uint32 Flash_Addr_Start, Uint32 Length)
{
    Uint16 i;
    Uint16 q, r ;
    Uint32 crcResult;
    Uint32 Addr_Start, Addr_Length;

    Addr_Start = Flash_Addr_Start;
    Addr_Length = Length * 2;
    // Step 1: Initialize the CRC object
    CRC.pMsgBuffer = (uint16_t *)Addr_Start;
    CRC.parity     = CRC_parity_even;
    CRC.crcResult  = 0;
    CRC.init       = (void (*)(void *))CRC_init32Bit;
    CRC.run        = (void (*)(void *))CRC_run32BitTableLookupC;

    CRC.seedValue  = INIT_CRC32;
    q = (uint16_t)((uint32_t)(Addr_Length & 0xFFFF0000) >> 16); // multiples of 65536
    // Since we can do a max of 65535 bytes at a time, we need to add q
    // to r to do the remainder
    r = (uint16_t)((Addr_Length & 0x0000FFFF)) + q; // modulus 65535

    // Step 2: Initialize the handle
    handleCRC = &CRC;

    // Step 3: Run the 8-bit table look-up CRC routine and save the result
    CRC.init(handleCRC);

    // Step 4: Reset a few elements of the CRC object
    CRC.crcResult  = 0;
    CRC.run        = (void (*)(void *))CRC_run32BitPoly1;

    // Run the CRC for 65535 bytes q times
    for(i = 0; i < q; i++)
    {
        //When CRC starts on low byte, it ends on a low byte, the next
        // set of 65535 bytes must start with high byte of the last address
        CRC.nMsgBytes  = 0xFFFF; // 65535 bytes
        CRC.run(handleCRC);
        CRC.seedValue  = CRC.crcResult;
        CRC.parity     ^= 1;
        CRC.pMsgBuffer = (uint16_t *)(Addr_Start + ((i+1)*0x8000 - CRC.parity));// - CRC.parity
    }
    // Run the CRC on the remaining r bytes
    CRC.nMsgBytes = r; // <= 65535 bytes
    CRC.run(handleCRC);

    crcResult = CRC.crcResult;

    return crcResult;
}