This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问我的F28035程序的TZFRC寄存器为什么不能把4路PWM波拉低?



专家您好,下面是我控制移相全桥电路的开环程序,F28035板子是我自己画的,在板子上放了一个开关进行对软启动程序控制,现在的问题是:当运行程序还未按下开关时,我使用TZFRC寄存器加了强制拉低语句,但是4路PWM波不能被拉到低电平(epwm3A发波  3B发波,EPWM6A为高,6B为低),当开关按下之后,PWM6A 6B开始发波。请专家帮我看一下,为什么在开关为按下去之前,4路pwm波为什么不能拉低?非常感谢您,麻烦您看看哪里有错误

interrupt void epwm3_isr(void);//interrupt关键字的作用是申明一个函数为中断函数,该中断函数的中断号为intr
void Init_EPwm3(void);
void Init_EPwm6(void);
void Init_Gpio(void);
Uint32 ss_count;
Uint16 ss_flag;
long temp1=0;

void Init_Gpio(void) //初始化GPIO

{
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO4=1; //设置GPIO4口为EPWM3A波形输出引脚
GpioCtrlRegs.GPADIR.bit.GPIO4=1; //设置GPIO4口方向为输出
GpioCtrlRegs.GPAMUX1.bit.GPIO5=1; //设置GPIO5口为EPWM3B波形输出引脚
GpioCtrlRegs.GPADIR.bit.GPIO5=1; //设置GPIO5口方向为输出

GpioCtrlRegs.GPAMUX1.bit.GPIO10=01; //设置GPIO10口为EPWM6A波形输出引脚
GpioCtrlRegs.GPADIR.bit.GPIO10=1; //设置GPIO10口方向为输出
GpioCtrlRegs.GPAMUX1.bit.GPIO11=01; //设置GPIO11口为EPWM6B波形输出引脚
GpioCtrlRegs.GPADIR.bit.GPIO11=1; //设置GPIO11口方向为输出

GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 0; // 0:GPIO 1:Peripheral
GpioCtrlRegs.GPADIR.bit.GPIO17 = 1; // 0:Input 1:Output

GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 0; // 0:GPIO 1:Peripheral
GpioCtrlRegs.GPADIR.bit.GPIO18 = 1; // 0:Input 1:Output


GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; // 0:GPIO 1:Peripheral
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 0; // 0:Input 1:Output
GpioCtrlRegs.GPBCTRL.bit.QUALPRD0 = 1;//两个机器周期检测一次
GpioCtrlRegs.GPBQSEL1.bit.GPIO34 = 2; //使用6次采样鉴定
// GpioCtrlRegs.GPAPUD.all = 0x0000; //上拉
EDIS;
}
/*
void initComp2out()
{
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO21 = 0; // Enable pullup on GPIO3(上拉电阻是做什么的?一般情况下都是会设置成使用上拉电阻模式)
GpioCtrlRegs.GPAMUX2.bit.GPIO21 = 3; // GPIO3 = GPIO3
GpioCtrlRegs.GPADIR.bit.GPIO21 = 1; // GPIO3 = output
EDIS;
}


void initComp2Gpio()//用于过压保护
{
EALLOW;
GpioCtrlRegs.AIOMUX1.bit.AIO4 = 2; // Configure AIO2 for CMP2A (analog input) operation
EDIS;
}

void initComp3Gpio()//用于过流保护
{
EALLOW;
GpioCtrlRegs.AIOMUX1.bit.AIO6 = 2; // Configure AIO4 for CMP3A (analog input) operation
EDIS;
}
*/
void Init_EPwm3(void)
{
// Initialization Timer
EPwm3Regs.TBPRD = 300; // Period = 2*300 TBCLK counts
EPwm3Regs.TBPHS. half.TBPHS= 0; // Set Phase register to zero
EPwm3Regs.TBCTR = 0; // clear TB counter
EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetric
EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Phase loading disabled
EPwm3Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm3Regs.TBCTL.bit.SYNCOSEL = 00;
EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // TBCLK = SYSCLKOUT
EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm3Regs.AQCTLA.bit.ZRO = AQ_SET; // set actions for EPWM1A
EPwm3Regs.AQCTLA.bit.PRD = AQ_CLEAR; //S1
EPwm3Regs.AQCTLB.bit.ZRO = AQ_CLEAR;
EPwm3Regs.AQCTLB.bit.PRD = AQ_SET; //S2
//
//Run Time
// = = = = = = = = = = = = = = = = = = = = = = = =
// EPwm1Regs.CMPA.half.CMPA = 360; // adjust duty for output EPWM1A
// EPwm1Regs.CMPB=75; // adjust duty for output EPWM1B 移向45度
EPwm3Regs.DBCTL.bit.OUT_MODE=DB_FULL_ENABLE; //11
EPwm3Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC; //10
EPwm3Regs.DBCTL.bit.IN_MODE=00; //选Epwm1A为下降沿和上升沿延迟输入源
EPwm3Regs.DBRED=30; //上升沿延迟时间
EPwm3Regs.DBFED=30; //下降沿延迟时间

EPwm3Regs.TZSEL.bit.OSHT1=1;
EPwm3Regs.TZCTL.bit.TZA=2;
EPwm3Regs.TZCTL.bit.TZB=2;


/*
// 过流、过压保护

Comp2Regs.DACVAL.bit.DACVAL =200; //过电压参考值
Comp3Regs.DACVAL.bit.DACVAL =270; //过电流参考值
//comp的输出控制,是否反相,是否同步?
Comp2Regs.COMPCTL.bit.CMPINV =0; //不反相,传送比较器的输出
Comp3Regs.COMPCTL.bit.CMPINV =0; //不反相,传送比较器的输出
Comp2Regs.COMPCTL.bit.SYNCSEL =0; //比较器输出被异步传送
Comp3Regs.COMPCTL.bit.SYNCSEL =0; //比较器输出被异步传送
//设置DC模块,comp1out(当短路时,comp1out的输出是1,否则输出是0)产生DCAEVT1的force信号
EALLOW;
EPwm3Regs.DCTRIPSEL.bit.DCAHCOMPSEL=DC_COMP2OUT; //COMP2OUT是数字比较A(DCAH)的输入选择位
EPwm3Regs.DCTRIPSEL.bit.DCBHCOMPSEL=DC_COMP3OUT;
EPwm3Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCAH_HI; //COMP3OUT输出为高电平,DCAL为任意值时,会产生DCAEVT1事件 DCAH = high, DCAL = don't care
EPwm3Regs.TZDCSEL.bit.DCBEVT1 = TZ_DCBH_HI;
EPwm3Regs.DCACTL.bit.EVT1SRCSEL =0; //DCAEVT1 Source Signal Select Source Is DCAEVT1 Signal
EPwm3Regs.DCBCTL.bit.EVT1SRCSEL =0;
EPwm3Regs.DCACTL.bit.EVT1FRCSYNCSEL =1; //DCAEVT1是异步信号,不进行同步,这时是不需要设置TZFRC[DCAEVT1]的,因为是两种使得DCAEVT1force产生的方式,要产生DCAEVT1force这个信号是可以直接用软件实现的。
EPwm3Regs.DCBCTL.bit.EVT1FRCSYNCSEL =1;
EDIS;
//封锁超前管PWM波
EALLOW;
EPwm3Regs.TZSEL.bit.DCAEVT1 = 1; //DCAEVT1是单次触发的故障源
EPwm3Regs.TZSEL.bit.DCBEVT1 = 1;
EPwm3Regs.TZCTL.bit.TZA =TZ_FORCE_LO; //DCAEVT1触发事件发生时,将EPWM1A设置成出错时变低
EPwm3Regs.TZCTL.bit.TZB =TZ_FORCE_LO; //DCBEVT1触发事件发生时,将EPWM1B设置成出错时变低
EPwm3Regs.TZEINT.bit.OST = 1; //使能综合的中断 Enable Interrupt generation; a one-shot trip event will cause a EPWMx_TZINT PIE interrupt
EDIS;
*/

//产生EPWM3INT3中断
EPwm3Regs.ETSEL.bit.INTSEL=ET_CTR_ZERO; //当时基计数器等于0时产生EPWM3INT1中断
EPwm3Regs.ETPS.bit.INTPRD =ET_3RD; //在第3个事件时产生中断
EPwm3Regs.ETSEL.bit.INTEN=1; //EPWM1 INT中断使能


}
void Init_EPwm6(void) //初始化EPWM2 开关管S3,S4
{
// Initialization Timer
EPwm6Regs.TBPRD = 300; // Period = 2*300 TBCLK counts
EPwm6Regs.TBPHS. half.TBPHS= 0; // Set Phase register to zero
EPwm6Regs.TBCTR = 0; // clear TB counter
EPwm6Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetric
EPwm6Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Phase loading disabled
EPwm6Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm6Regs.TBCTL.bit.SYNCOSEL = 00;
EPwm6Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // TBCLK = SYSCLKOUT
EPwm6Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm6Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm6Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm6Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm6Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm6Regs.AQCTLA.bit.CAU = AQ_SET; // set actions for EPWM3A
EPwm6Regs.AQCTLA.bit.CBD = AQ_CLEAR; //S5
EPwm6Regs.AQCTLB.bit.CAU = AQ_CLEAR;
EPwm6Regs.AQCTLB.bit.CBD = AQ_SET; //S6
//
//Run Time
// = = = = = = = = = = = = = = = = = = = = = = = =
//EPwm6Regs.CMPA.half.CMPA =0;
//EPwm6Regs.CMPB=0;


EPwm6Regs.DBCTL.bit.OUT_MODE=DB_FULL_ENABLE; //11
EPwm6Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC; //10
EPwm6Regs.DBCTL.bit.IN_MODE=0; //选Epwm2A为下降沿和上升沿延迟输入源
EPwm6Regs.DBRED=30; //上升沿延迟时间
EPwm6Regs.DBFED=30; //下降延迟时间

EPwm6Regs.TZSEL.bit.OSHT1=1;
EPwm6Regs.TZCTL.bit.TZA=2;
EPwm6Regs.TZCTL.bit.TZB=2;

/*
//过流、过压保护
Comp2Regs.DACVAL.bit.DACVAL =200; //过电压参考值
Comp3Regs.DACVAL.bit.DACVAL =270; //过电流参考值
//comp的输出控制,是否反相,是否同步?
Comp2Regs.COMPCTL.bit.CMPINV =0; //不反相,传送比较器的输出
Comp3Regs.COMPCTL.bit.CMPINV =0; //不反相,传送比较器的输出
Comp2Regs.COMPCTL.bit.SYNCSEL =0; //比较器输出被异步传送
Comp3Regs.COMPCTL.bit.SYNCSEL =0; //比较器输出被异步传送
//设置DC模块,comp1out(当短路时,comp1out的输出是1,否则输出是0)产生DCAEVT1的force信号
EALLOW;
EPwm6Regs.DCTRIPSEL.bit.DCAHCOMPSEL=DC_COMP2OUT; //COMP2OUT是数字比较A(DCAH)的输入选择位
EPwm6Regs.DCTRIPSEL.bit.DCBHCOMPSEL=DC_COMP3OUT;
EPwm6Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCAH_HI; //COMP2OUT输出为高电平,DCAL为任意值时,会产生DCAEVT1事件 DCAH = high, DCAL = don't care
EPwm6Regs.TZDCSEL.bit.DCBEVT1 = TZ_DCBH_HI;
EPwm6Regs.DCACTL.bit.EVT1SRCSEL =0; //DCAEVT1 Source Signal Select Source Is DCAEVT1 Signal
EPwm6Regs.DCBCTL.bit.EVT1SRCSEL =0;
EPwm6Regs.DCACTL.bit.EVT1FRCSYNCSEL =1; //DCAEVT1是异步信号,不进行同步,这时是不需要设置TZFRC[DCAEVT1]的,因为是两种使得DCAEVT1force产生的方式,要产生DCAEVT1force这个信号是可以直接用软件实现的。
EPwm6Regs.DCBCTL.bit.EVT1FRCSYNCSEL =1;
EDIS;
//是否封锁滞后管PWM波
EALLOW;
EPwm6Regs.TZSEL.bit.DCAEVT1 = 1; //DCAEVT1是单次触发的故障源
EPwm6Regs.TZSEL.bit.DCBEVT1 = 1;
EPwm6Regs.TZCTL.bit.TZA =TZ_FORCE_LO; //DCAEVT1触发事件发生时,将EPWM1A设置成出错时变低
EPwm6Regs.TZCTL.bit.TZB =TZ_FORCE_LO; //DCBEVT1触发事件发生时,将EPWM1B设置成出错时变低
EPwm6Regs.TZEINT.bit.OST = 1; //使能综合的中断 Enable Interrupt generation; a one-shot trip event will cause a EPWMx_TZINT PIE interrupt
EDIS;
*/
}

void delay()
{
Uint16 i=0, j=0;
for(i=0; i<1000; i++)
for(j=0; j<10; j++);
}


void main(void)
{


InitSysCtrl();

Init_Gpio(); // Skipped for this example初始化GPIO口,包括ePWM1,ePWM2,ePWM3,ePWM4,
/*
// For this case just init GPIO pins for ePWM1, ePWM2, and TZ1 pins
initComp2out();
initComp2Gpio();//设置AIO2口作为COMP2A的端口
initComp3Gpio();//设置AIO4口作为COMP3A的端口
//GPIO4();
*/
// Disable CPU interrupts
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();

EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.EPWM3_INT = &epwm3_isr;//&表示取地址,此句表示设置EPWM1_INT中断服务程序的入口地址为epwm1_isr
EDIS;

IER |= M_INT3;

PieCtrlRegs.PIEIER3.bit.INTx3 = 1;
EINT; // Enable Global interrupt INTM
ERTM;

EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;//停止每个已使能EPWM模块内的时基时钟(TBCLK)(默认状态)。

SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1; // Enable Clock to the ADC
AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; // Comparator shares the internal BG reference of the ADC, must be powered even if ADC is unused

SysCtrlRegs.PCLKCR3.bit.COMP2ENCLK = 1; // Enable clock to the Comparator 1 block
SysCtrlRegs.PCLKCR3.bit.COMP3ENCLK = 1; // Enable clock to the Comparator 2 block
Comp2Regs.COMPCTL.bit.COMPDACEN = 1; // Power up Comparator 1 locally 比较器/DAC逻辑上电
Comp3Regs.COMPCTL.bit.COMPDACEN = 1; // Power

Comp2Regs.COMPCTL.bit.COMPSOURCE =0; //使用DAC内部基准 比较器的负极输入连接到内部ADC
Comp3Regs.COMPCTL.bit.COMPSOURCE =0; //使用DAC内部基准 比较器的负极输入连接到内部ADC

EDIS; //但是,如果PCLKCR1寄存器的EPWM时钟使能位被置位,那么EPWM模块仍然由SYSCLKOUT来计时,即使TBCLKSYNC为0。


Init_EPwm3();
Init_EPwm6();


EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;//所有已使能的EPWM模块的时钟在已校准的TBCLK的第一个上升沿启动。为了得到完美同
//步的TBCLK,每个EPWM模块的TBCLK寄存器中的预分频器位必须设置相同。使能EPWM时钟的正确过程如下所示:在PCLKCR1寄存器中
//使能EPWM模块时钟;将TBCLKSYNC设置为0;配置预分频器值和EPWM模式;将TBCLKSYNC设置为1。
EDIS;

Restart_Begining:

ss_count=0;
ss_flag=0;
EPwm6Regs.CMPA.half.CMPA =0;
EPwm6Regs.CMPB=0;
EPwm6Regs.TZFRC.bit.OST = 1;
EPwm3Regs.TZFRC.bit.OST = 1;


//检测开关是否闭合,开始软启动
while(1)
{
if(GpioDataRegs.GPBDAT.bit.GPIO34 == 0)
{
delay();
if(GpioDataRegs.GPBDAT.bit.GPIO34 == 0) break;
}
}
ss_flag = 1;

// Step 7. IDLE loop. Just sit and loop forever (optional):
for(;;)
{
if(GpioDataRegs.GPBDAT.bit.GPIO34 == 1)
{
delay();
if(GpioDataRegs.GPBDAT.bit.GPIO34 == 1)
goto Restart_Begining;
}


}

}

interrupt void epwm3_isr(void)
{


if(ss_flag == 1)
{
if(ss_count<=307200)
{
ss_count++;
temp1=(long)((ss_count)>>11);


EPwm6Regs.CMPA.half.CMPA =300-temp1;
EPwm6Regs.CMPB=temp1;

}

}


EPwm3Regs.ETCLR.bit.INT = 1; //清除EPWM3 INT的中断标志位
// Acknowledge this interrupt to receive more interrupts from group 3
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
EINT;
}

  • 因为你没有加eallow去保护,TZFRC是受保护寄存器

  • en  太谢谢您了  原因找到了 同时还需要使用 EPwm3Regs.TZCLR.bit.OST = 1;  这个话来清除软件强制的作用

  • 恩恩 谢谢了问题解决了

  • 您好,今天我调试,带软启动的电压闭环程序,为什么这样写程序不能实现,在按下开关后软启动程序先起作用,然后在开始PI运算的功能呢?麻烦您帮我看一下哪地方写的不合适?

    Uint16 Voltage1[10];
    Uint16 Voltage2[10];
    Uint16 ConversionCount;
    Uint16 count;//用以表示EPWM1INT中断开始工作
    Uint32 ss_count;
    Uint16 ss_flag;

    _iq U_Kp=_IQ(1),U_Ki=_IQ(0); //Ki=12000*Tsample Ki乘以采样周期定标
    _iq Ue0=0,Ue1=0,Ue2=0,Uref=0,Up=0,Ui=0,Uo0=0,Uo1=0,Uo2=0,Ureal=0;
    long U1,I1;
    long CA,CB;
    long temp1,temp2;
    int U_Ref= 265 ;


    void Init_Gpio(void) //初始化GPIO

    {
    EALLOW;
    GpioCtrlRegs.GPAMUX1.bit.GPIO4=1; //设置GPIO4口为EPWM3A波形输出引脚
    GpioCtrlRegs.GPADIR.bit.GPIO4=1; //设置GPIO4口方向为输出
    GpioCtrlRegs.GPAMUX1.bit.GPIO5=1; //设置GPIO5口为EPWM3B波形输出引脚
    GpioCtrlRegs.GPADIR.bit.GPIO5=1; //设置GPIO5口方向为输出

    GpioCtrlRegs.GPAMUX1.bit.GPIO10=01; //设置GPIO10口为EPWM6A波形输出引脚
    GpioCtrlRegs.GPADIR.bit.GPIO10=1; //设置GPIO10口方向为输出
    GpioCtrlRegs.GPAMUX1.bit.GPIO11=01; //设置GPIO11口为EPWM6B波形输出引脚
    GpioCtrlRegs.GPADIR.bit.GPIO11=1; //设置GPIO11口方向为输出

    GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 0; // 0:GPIO 1:Peripheral
    GpioCtrlRegs.GPADIR.bit.GPIO17 = 1; // 0:Input 1:Output

    GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 0; // 0:GPIO 1:Peripheral
    GpioCtrlRegs.GPADIR.bit.GPIO18 = 1; // 0:Input 1:Output


    GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; // 0:GPIO 1:Peripheral
    GpioCtrlRegs.GPBDIR.bit.GPIO34 = 0; // 0:Input 1:Output
    GpioCtrlRegs.GPBCTRL.bit.QUALPRD0 = 1;//两个机器周期检测一次
    GpioCtrlRegs.GPBQSEL1.bit.GPIO34 = 2; //使用6次采样鉴定
    GpioCtrlRegs.GPAPUD.all = 0x0000; //上拉
    EDIS;
    }
    /*
    void GPIO0()
    {
    EALLOW;
    GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0; // Enable pullup on GPIO3(上拉电阻是做什么的?一般情况下都是会设置成使用上拉电阻模式)
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; // GPIO0 = GPIO0
    GpioCtrlRegs.GPADIR.bit.GPIO0 = 1; // GPIO0 = output
    EDIS;
    }

    void Init_Adc(void) //初始化ADC模块
    {
    EALLOW;
    AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; // Power ADC BG ADCCTL1的位6 带隙上电
    AdcRegs.ADCCTL1.bit.ADCREFPWD = 1; // Power reference ADCCTL1的位5 参考上电
    AdcRegs.ADCCTL1.bit.ADCPWDN = 1; // Power ADC ADCCTL1的位7 Power up rest of ADC除带隙和参考上电以外的上电
    AdcRegs.ADCCTL1.bit.ADCENABLE = 1; // Enable ADC ADCCTL1的位14
    AdcRegs.ADCCTL1.bit.ADCREFSEL = 0; // Select interal BG 建议使用内部基准 内部基准一般就是指3.3v ( Digital Value = 4096 [(Input – VREFLO)/3.3v] when 0v < Input < 3.3v)


    DELAY_US(ADC_usDELAY);

    //选择序列采样模式
    AdcRegs.ADCSAMPLEMODE.bit.SIMULEN0=0; //SOC0和SOC1
    AdcRegs.ADCSAMPLEMODE.bit.SIMULEN2=0; //SOC2和SOC3
    AdcRegs.ADCSAMPLEMODE.bit.SIMULEN4=0; //SOC4和SOC5
    AdcRegs.ADCSAMPLEMODE.bit.SIMULEN6=0; //SOC6和SOC7


    AdcRegs.ADCSOC7CTL.bit.CHSEL = 7; //set SOC7 channel select to ADCINA7 SOC1选择ADCINA1通道 A1通道采U1 SOC1的结果存于ADCRETSULT1寄存器中


    AdcRegs.ADCSOC7CTL.bit.TRIGSEL = 9; // SOC7的触发源选择EPWM3A


    AdcRegs.ADCSOC7CTL.bit.ACQPS = 6; //set SOC7 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1) SOC1的采样窗口为7个周期长度

    EDIS;
    // Assumes ePWM1 clock is already enabled in InitSysCtrl();
    EPwm3Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group 使能ADC开始转换A(EPEMxSOCA)脉冲
    EPwm3Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount 使能事件,当定时器递增时时间基准计数器等于CMPA
    EPwm3Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event 在第一个件上生成ePWMxSOCA脉冲:ETPS[SOCACNT]=0,1

    }

    void Init_EPwm3(void)
    {
    // Initialization Timer
    EPwm3Regs.TBPRD = 300; // Period = 2*300 TBCLK counts
    EPwm3Regs.TBPHS. half.TBPHS= 0; // Set Phase register to zero
    EPwm3Regs.TBCTR = 0; // clear TB counter
    EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetric
    EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Phase loading disabled
    EPwm3Regs.TBCTL.bit.PRDLD = TB_SHADOW;
    EPwm3Regs.TBCTL.bit.SYNCOSEL = 00;
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // TBCLK = SYSCLKOUT
    EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR = Zero
    EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR = Zero
    EPwm3Regs.AQCTLA.bit.ZRO = AQ_SET; // set actions for EPWM1A
    EPwm3Regs.AQCTLA.bit.PRD = AQ_CLEAR; //S1
    EPwm3Regs.AQCTLB.bit.ZRO = AQ_CLEAR;
    EPwm3Regs.AQCTLB.bit.PRD = AQ_SET; //S2
    //
    //Run Time
    // = = = = = = = = = = = = = = = = = = = = = = = =
    // EPwm1Regs.CMPA.half.CMPA = 360; // adjust duty for output EPWM1A
    // EPwm1Regs.CMPB=75; // adjust duty for output EPWM1B 移向45度
    EPwm3Regs.DBCTL.bit.OUT_MODE=DB_FULL_ENABLE; //11
    EPwm3Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC; //10
    EPwm3Regs.DBCTL.bit.IN_MODE=00; //选Epwm1A为下降沿和上升沿延迟输入源
    EPwm3Regs.DBRED=30; //上升沿延迟时间
    EPwm3Regs.DBFED=30; //下降沿延迟时间

    EPwm3Regs.TZSEL.bit.OSHT1=1;
    EPwm3Regs.TZCTL.bit.TZA=TZ_FORCE_LO;
    EPwm3Regs.TZCTL.bit.TZB=TZ_FORCE_LO;

    //产生EPWM3INT3中断
    EPwm3Regs.ETSEL.bit.INTSEL=ET_CTR_ZERO; //当时基计数器等于0时产生EPWM3INT1中断
    EPwm3Regs.ETPS.bit.INTPRD =ET_3RD; //在第3个事件时产生中断
    EPwm3Regs.ETSEL.bit.INTEN=1; //EPWM1 INT中断使能


    }
    void Init_EPwm6(void) //初始化EPWM2 开关管S3,S4
    {
    // Initialization Timer
    EPwm6Regs.TBPRD = 300; // Period = 2*300 TBCLK counts
    EPwm6Regs.TBPHS. half.TBPHS= 0; // Set Phase register to zero
    EPwm6Regs.TBCTR = 0; // clear TB counter
    EPwm6Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetric
    EPwm6Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Phase loading disabled
    EPwm6Regs.TBCTL.bit.PRDLD = TB_SHADOW;
    EPwm6Regs.TBCTL.bit.SYNCOSEL = 00;
    EPwm6Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // TBCLK = SYSCLKOUT
    EPwm6Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    EPwm6Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm6Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm6Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR = Zero
    EPwm6Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR = Zero
    EPwm6Regs.AQCTLA.bit.CAU = AQ_SET; // set actions for EPWM3A
    EPwm6Regs.AQCTLA.bit.CBD = AQ_CLEAR; //S5
    EPwm6Regs.AQCTLB.bit.CAU = AQ_CLEAR;
    EPwm6Regs.AQCTLB.bit.CBD = AQ_SET; //S6
    //
    //Run Time
    // = = = = = = = = = = = = = = = = = = = = = = = =
    //EPwm6Regs.CMPA.half.CMPA =0;
    //EPwm6Regs.CMPB=0;


    EPwm6Regs.DBCTL.bit.OUT_MODE=DB_FULL_ENABLE; //11
    EPwm6Regs.DBCTL.bit.POLSEL=DB_ACTV_HIC; //10
    EPwm6Regs.DBCTL.bit.IN_MODE=0; //选Epwm2A为下降沿和上升沿延迟输入源
    EPwm6Regs.DBRED=30; //上升沿延迟时间
    EPwm6Regs.DBFED=30; //下降延迟时间

    EPwm6Regs.TZSEL.bit.OSHT1=1;
    EPwm6Regs.TZCTL.bit.TZA=TZ_FORCE_LO;
    EPwm6Regs.TZCTL.bit.TZB=TZ_FORCE_LO;



    }

    void delay()
    {
    Uint16 i=0, j=0;
    for(i=0; i<1000; i++)
    for(j=0; j<10; j++);
    }

    void main(void)
    {

    InitSysCtrl();
    Init_Gpio();
    // For this case just init GPIO pins for ePWM1, ePWM2, and TZ1 pins


    DINT;
    InitPieCtrl(); // 初始化 PIE 控制寄存器
    IER = 0x0000; // 禁止 CPU 中断
    IFR = 0x0000; //清除 CPU 中断标志
    InitPieVectTable(); // 初始化 中断向量表

    EALLOW;
    PieVectTable.EPWM3_INT = &epwm3_isr;//&表示取地址,此句表示设置EPWM3_INT中断服务程序的入口地址为epwm1_isr

    EDIS;
    IER |= M_INT3;
    // Enable EPWM INT1 in the PIE: Group 3 interrupt 1,且使能group 1 interrupt 1
    PieCtrlRegs.PIEIER3.bit.INTx3 = 1;
    EINT; // Enable Global interrupt INTM
    ERTM; // Enable Global realtime interrupt DBGM

    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;//停止每个已使能EPWM模块内的时基时钟(TBCLK)(默认状态)。

    EDIS; //但是,如果PCLKCR1寄存器的EPWM时钟使能位被置位,那么EPWM模块仍然由SYSCLKOUT来计时,即使TBCLKSYNC为0。

    delay();
    Init_Adc(); // For this example, init the ADC
    Init_EPwm3();
    Init_EPwm6();

    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;//所有已使能的EPWM模块的时钟在已校准的TBCLK的第一个上升沿启动。为了得到完美同
    //步的TBCLK,每个EPWM模块的TBCLK寄存器中的预分频器位必须设置相同。使能EPWM时钟的正确过程如下所示:在PCLKCR1寄存器中
    //使能EPWM模块时钟;将TBCLKSYNC设置为0;配置预分频器值和EPWM模式;将TBCLKSYNC设置为1。
    EDIS;

    Restart_Begining:

    GpioDataRegs.GPADAT.bit.GPIO17 = 0;
    DELAY_US(10L);
    GpioDataRegs.GPADAT.bit.GPIO18 = 0;


    CA=0,CB=0;
    count=0;
    temp1=0;
    temp2=0;
    ss_count=0;
    ss_flag=0;
    EPwm6Regs.CMPA.half.CMPA =0;
    EPwm6Regs.CMPB=0;
    EALLOW;
    EPwm6Regs.TZFRC.bit.OST = 1;
    EPwm3Regs.TZFRC.bit.OST = 1;
    EDIS;


    //检测开关是否闭合,开始软启动
    while(1)
    {
    if(GpioDataRegs.GPBDAT.bit.GPIO34 == 0)
    {
    delay();
    if(GpioDataRegs.GPBDAT.bit.GPIO34 == 0) break;
    }
    }
    ss_flag = 1;


    EALLOW;
    EPwm3Regs.TZCLR.bit.OST = 1;
    EPwm6Regs.TZCLR.bit.OST = 1;
    EDIS;


    // Step 7. IDLE loop. Just sit and loop forever (optional):
    for(;;)
    {
    if(GpioDataRegs.GPBDAT.bit.GPIO34 == 1)
    {
    delay();
    if(GpioDataRegs.GPBDAT.bit.GPIO34 == 1)
    goto Restart_Begining;
    }


    }

    }


    interrupt void epwm3_isr(void)
    {


    if(ss_flag == 1)
    {
    if(ss_count<=307200)
    {
    ss_count++;
    temp1=(long)((ss_count)>>11);

    EPwm6Regs.CMPA.half.CMPA =300-temp1;
    EPwm6Regs.CMPB=temp1;

    }
    }


    U1= AdcResult.ADCRESULT7; //U1电压, A7通道采U1
    Voltage1[ConversionCount] = AdcResult.ADCRESULT7; //ADC的最近10次采样结果放在Voltage1数组中

    // If 10 conversions have been logged, start over
    if(ConversionCount == 9)
    {
    ConversionCount = 0;

    }
    else //AD采样值是经过10次求平均得到的

    {
    ConversionCount++;
    }


    //pi程序
    Ureal=_IQ(U1);

    Uref=_IQ(U_Ref); //300缩放为2.3,对应数字量为2855

    Ue1=Uref-Ureal ;

    Ue2=Ue1-Ue0; //两者的误差

    Up=_IQmpy(U_Kp,Ue2);

    Ui=_IQmpy(U_Ki,Ue1);

    Uo1=Uo0+Up+Ui;

    Ue0=Ue1;

    Uo0=Uo1;

    if(Uo1>=_IQ(EPwm3Regs.TBPRD*0.9)) Uo1 =_IQ(EPwm3Regs.TBPRD*0.9); // PI 输出上限幅

    if(Uo1<=_IQ(1)) Uo1 =_IQ(1); // PI 输出下限幅

    temp2=(long)((Uo1)>>18); //调制波得到数据

    if ( temp2>=270) { temp2=270; EPwm6Regs.CMPA.half.CMPA = temp2; EPwm6Regs.CMPB=300-temp2; }
    else if ( temp2<=0) { temp2=1; EPwm6Regs.CMPA.half.CMPA = temp2; EPwm6Regs.CMPB=300-temp2; } //设置移向角范围为0.6度到90

    CA=temp2;
    CB=300-temp2;
    EPwm6Regs.CMPA.half.CMPA =CA; //移向角
    EPwm6Regs.CMPB=CB;

    // I1= AdcResult.ADCRESULT0; //I1电压, A0通道采I1

    count++;
    GpioDataRegs.GPATOGGLE.bit.GPIO0=1;
    /*

    */
    GpioDataRegs.GPATOGGLE.bit.GPIO0=0;
    EPwm3Regs.ETCLR.bit.INT = 1; //清除EPWM1 INT的中断标志位
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;

    }

  • 具体是什么问题,怎么不能实现?

  • 问题是:我按下控制软启动的开关后,软启动程序和PI运算程序一起运算,这样应该不对.  我想要这样的功能:当按下控制软启动开关后,只有软启动程序起作用,等软启动完毕后,PI再开始运算。  麻烦您看一下为什么不能实现我想要的这个功能?

  • 问题是:我按下控制软启动的开关后,软启动部分和PI运算一起起作用,这样应该不对。我想要实现的功能是:按下控制软启动的开关后,首先只有软启动程序起作用,当软启动完毕后,PI再开始运算调节占空比。为什么不能实现我想要的这个功能呢?麻烦您看一下哪里有问题?