This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377的PPB中的zero crossing怎么用?



您好!

    如题,电路上将VREFHI接+2.5V,VREFLO接-2.5V,再配置某个PPB的zero corssing中断,这样就能用了么?如果电路上,在ADC信号输入时加了+1.25的偏置,VREFHI接+2.5V,VREFLO接GND,这样还能使能zero crossing功能么?

  • VREFLO不能接-2.5V,zero corssing是接在offset calculate后面,所以需要把你的采样值减去offset后,会自动检测PPB result里面的值是否是负数,是的话就会置位zero crossing 位。

    所以只有VREFHI接+2.5V,VREFLO接GND才可以用