This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28069的USB接口设计

Other Parts Discussed in Thread: CONTROLSUITE

大家好!

        首先说一下:我下载了controlSUITE了,在里面搜索USB的资料,没有找到以下这个帖子所说“TI提供的原理图”;而在知网里面28069的资料不多;耐着性子把USB模块的Datasheet看了一遍,英文版的TI支持论坛有1份28069的控制卡原理图,详见附件,我也看了,还是有点疑惑。

       www.deyisupport.com/.../11241.aspx

       所以,在这里弱弱地请教一下28069的USB接口设计。

        1.首先要实现的功能是:28069与PC的通信。

        (1)这时候,28069是工作在device模式吧?其USB模块还需要VBUS供电么?应该是self-powered吧?

        (2)对于VBUS,我一定需要用1个GPIO连100K的电阻接电脑的USB接口么?因为我的GPIO已经全部分配完了,如果一定需要的话,我再裁减部分功能。

        (3)对于D+的上拉,用内部的上拉就足够么?

        2.不重要的功能(不一定要实现):28069将数据写入U盘。

         这个功能用28069能够实现么?如果可以的话,能否推荐一个接口电路,或者提供设计资料。

       刚接触28069,比较菜。

       麻烦大家了!

  • 电脑肯定是主机   c2000是设备   VBUS有主机提供    你可以使用

    也可以不使用    

    USB的差分上不用上下拉  

    关于C2000做主的不太了解    

    controlSUTIE里面只有EVM板提供原理图

  • (1)这时候,28069是工作在device模式吧?其USB模块还需要VBUS供电么?应该是self-powered吧?

    (2)对于VBUS,我一定需要用1个GPIO连100K的电阻接电脑的USB接口么?因为我的GPIO已经全部分配完了,如果一定需要的话,我再裁减部分功能                 

     Most applications do not have a need to monitor VBus, and because of this, a dedicated VBus monitoring
    pin was not included on this processor. If you are designing a bus-powered device application or an
    embedded host application, you do NOT need to monitor VBus. If you are designing a self-powered
    device, you will however, need to actively monitor the state of the VBus pin in order to ensure compliance
    with the USB specification. In Section 7.1.5 and Section 7.2.1 of the USB Specification Revision 2.0™ it is
    stated respectively that:

    看你的需求,可以加也可以不加,看是不是self power

            (3)对于D+的上拉,用内部的上拉就足够么?

                     是的,足够了

            2.不重要的功能(不一定要实现):28069将数据写入U盘。

             这个功能用28069能够实现么?如果可以的话,能否推荐一个接口电路,或者提供设计资料。

    这个功能不能实现,因为要给U盘写数据,F28069就是host,F28069的USB不能做HOST,你又要作为PC的device,这样就是OTG

  • 谢谢您的回复!

    我给28069U肯定是有3.3V模拟供电和数字供电的啦,这算是self-powered么?

    Datasheet上说大部分应用不需要监控Vbus,所以我想:难道我的应用不在常见应用的范围内?