各位老师好,我正在学习f28035,用的controlSUITE中的例程,我看到程序中都是这么用时钟 的,先把程序粘贴如下。为什么在系统中要设置时钟在下面这几个函数之间一直循环,作用是什么?另外系统中断是采用定时器中断还是CPU中断,这个在哪有配置呢?
非常感谢!!!
void A0(void)
{
if(CpuTimer0Regs.TCR.bit.TIF == 1)
{
CpuTimer0Regs.TCR.bit.TIF = 1;
//-----------------------------------------------------------
(*A_Task_Ptr)(); // jump to an A Task (A1,A2,A3,...)
//-----------------------------------------------------------
VTimer0[0]++; // virtual timer 0, instance 0 (spare)
SerialCommsTimer++;
}
Alpha_State_Ptr = &B0; // Comment out to allow only A tasks
}
void B0(void)
{
if(CpuTimer1Regs.TCR.bit.TIF == 1)
{
CpuTimer1Regs.TCR.bit.TIF = 1;
//-----------------------------------------------------------
(*B_Task_Ptr)(); // jump to a B Task (B1,B2,B3,...)
//-----------------------------------------------------------
VTimer1[0]++; // virtual timer 1, instance 0 (spare)
}
Alpha_State_Ptr = &C0; // Allow C state tasks
}
void C0(void)
{
if(CpuTimer2Regs.TCR.bit.TIF == 1)
{
CpuTimer2Regs.TCR.bit.TIF = 1;
//-----------------------------------------------------------
(*C_Task_Ptr)(); // jump to a C Task (C1,C2,C3,...)
//-----------------------------------------------------------
VTimer2[0]++; //virtual timer 2, instance 0 (spare)
}
Alpha_State_Ptr = &A0; // Back to State A0
}
//=================================================================================
// A - TASKS (executed in every 1 msec)
//=================================================================================
//--------------------------------------------------------
void A1(void) // SPARE (not used)
{
if (Disable==1)
{
EALLOW;
EPwm1Regs.TZFRC.bit.OST=1;
EPwm2Regs.TZFRC.bit.OST=1;
EPwm3Regs.TZFRC.bit.OST=1;
EPwm4Regs.TZFRC.bit.OST=1;
EDIS;
}
A_Task_Ptr = &A2;
}
void A2(void) // SPARE (not used)
{ //the next time CpuTimer0 'counter' reaches Period value go to A3
A_Task_Ptr = &A3;
}
void A3(void) // SPARE (not used)
{ //the next time CpuTimer0 'counter' reaches Period value go to A1
A_Task_Ptr = &A1;
}
//=================================================================================
// B - TASKS (executed in every 5 msec)
//=================================================================================
void B1(void) // Toggle GPIO-00
{ //the next time CpuTimer1 'counter' reaches Period value go to B2
B_Task_Ptr = &B2;
}
void B2(void) // SPARE
{//the next time CpuTimer1 'counter' reaches Period value go to B3
B_Task_Ptr = &B3;
}
void B3(void) // SPARE
{ //the next time CpuTimer1 'counter' reaches Period value go to B1
B_Task_Ptr = &B1;
//-----------------
}
//=================================================================================
// C - TASKS (executed in every 50 msec)
//=================================================================================
void C1(void) // Toggle GPIO-34
{
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; // Blink LED
//-----------------
//the next time CpuTimer2 'counter' reaches Period value go to C2
C_Task_Ptr = &C2;
}
void C2(void) // SPARE
{ //the next time CpuTimer2 'counter' reaches Period value go to C3
C_Task_Ptr = &C3;
}
void C3(void) // SPARE
{ //the next time CpuTimer2 'counter' reaches Period value go to C1
C_Task_Ptr = &C1;
}