This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

单电流环矢量控制斜坡升速------请问这个问题大家有会的吗?急急急



  • 各位老师好,我在用controlSUITE中的矢量控制程序。在测试单电流环矢量控制时,需要用到斜坡升速模块,请问参数StepAngleMax为什么这么计算呢?下图为StepAngleMax的计算公式。

    斜坡升速信号产生模块的程序如下:

    #define RG_MACRO(v) \
    \
    /* Compute the angle rate */ \
    v.Angle += _IQmpy(v.StepAngleMax,v.Freq); \
    \
    /* Saturate the angle rate within (-1,1) */ \
    if (v.Angle>_IQ(1.0)) \
    v.Angle -= _IQ(1.0); \
    else if (v.Angle<_IQ(-1.0)) \
    v.Angle += _IQ(1.0); \
    \
    /* Compute the ramp output */ \
    v.Out = _IQmpy(v.Angle,v.Gain) + v.Offset; \
    /* Saturate the ramp output within (-1,1) */ \
    if (v.Out>_IQ(1.0)) \
    v.Out -= _IQ(1.0); \
    else if (v.Out<_IQ(-1.0)) \
    v.Out += _IQ(1.0);

    #endif // __RAMPGEN_H__

     
  • 举人2485分

    T是相邻两次stepAngle程序执行的间隔时间,BASE_FREQ是IQ(1)代表的最快转速值。因为1/BASE_FREQ是转一圈的时间,所以 T / (1/BASE_FREQ)代表间隔时间转过的角度也就是stepAngle。

     
  • 举人1175分

    您好!1/BASE_FREQ是转一圈的时间的话,那么BASE_FREQ设定为200hz的话,则BASE_FREQ对应的最快转速值为200r/s,即为12000r/s?但此时对应的实际最高转速为3000r/s,这个怎么解释呢?

    非常感谢!!!