This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

f28m35中ADC通道互通有什么用处?



ADC2 channel A1 is internally connected to ADC1 channel A0,  ADC1 channel A1 is internally connected to ADC2 channel A0.

ADC2 channel B1 is internally connected to ADC1 channel B0,  and ADC1 channel B1 is internally connected to ADC2 channel B0.

共4处。

  • 简单来说,可以理解为有两个好处:

    1. 增加了灵活性,在一个硬件设计完成后,仍然可以通过软件进行选择而勿需改板以达到切换通道的目的;

    2. 多通道采样同一信号的硬件实现,可以增强冗余度和减小误差,比如你可以同时用两个通道采集同一信号(因为有两个ADC转换模块),在软件上进行处理,当两者的差值在一定范围内时,认为是准确的,否则需要再处理,或再采集,或者直接丢弃该次采样,从而提高精度。