This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377D的can_loopback_interrupt_cpu1程序调试问题



各位好!

我最近在用28377D调试CAN这一块,硬件是28377D的官网开发板,自己外加的电路输出CAN_H和CAN_L,然后外接CAN收发器,可在电脑上观测总线上的收发数据;软件是用controlsuit中的28377D的v160版本的例程can_loopback_interrupt_cpu1。例程中使用的是外部回环测试模式,在芯片的Tx端我用示波器可以看到发送信号,但是通过CAN收发器,在电脑上看不到发送出的数据。

我个人分析的几个问题点:

1.外部回环测试模式下,只是硬件测试,是不是数据信号只能在CAN内核部分,不能外发?但是我在Tx端检测到信号,我在想有信号就应该能外发出去吧;

2.因暂时硬件这块资源比较缺少,我只是用了一块28377D的板子,也就是说总线上只有这一台设备。我之前有看到过说总线上至少要有两台设备,那我现在只有一台会不会有很大影响,我只是看Tx端的数据;

3.测试模式的问题,我将测试模式改为DAR模式或者是ABO模式,但是造成的后果就是连Tx和Rx的中断都进不了了

因初学28377D的CAN功能,之前没有接触过通信这一块,很多地方可能是我的理解有误,还请各位帮忙指导一下,看问题是出在什么地方了,谢谢!