This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP2808 EPWM4 寄存器写不进去



您好,我们使用DSP2808,在设置寄存器的时候,EPWM1、EPWM2、EPWM3、EPWM4采用相同的设置,但是EPWM1、EPWM2的寄存器能够写入,而EPWM4的寄存器写不进去。请教,谢谢!!!

  • 1. 是EPWM4所有的寄存器还是部分?EPWM5可以吗?

    2. 是否配置完全一样?请对比检查代码;

    3. 确保时钟是打开的;

    4. 确保有些寄存器是EALLOW使能的;

    5. 可以在观察窗口直接输入该寄存器地址,双击其值手动修改,回车查看是否生效。

  • 找到解决的方法了吗,我这边也碰到了一样的问题,EPWM4,5,6都不能用,配置和1,2,3, 是一样的,技术论坛给的解答我试了试都不行