This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS6.1版本C2000编译器28377D器件无法支持__attribute__问题,移植EtherCAT从站代码,无法编译成功



CCS版本:6.1

DSP:28377D

问题:移植EtherCAT从站代码,代码中带有巨多的__attribute__((aligned(1), packed))宏定义,在CCS6.1上也勾选了GCC选项(Build->advanced options->language options->enable support for gcc externsions),重新编译后仍旧存在如下提示:

\EtherCAT\include\esc.h", line 167: error #1167: invalid attribute for "struct <unnamed>"

难道C2000不支持__attribute__编译么??

  • 可以把167行附近的代码都贴出来看一下吗?另外,编译器版本是多少?

  • 代码如下:

    /**
    STRUCT_PACKED_START: Is defined before the typedef struct construct to pack the generic structures if necessary */
    #ifndef STRUCT_PACKED_START
    #define STRUCT_PACKED_START
    #endif

    /**
    STRUCT_PACKED_END: Is defined after the typedef struct {} construct to pack the generic structures if necessary */
    #ifndef STRUCT_PACKED_END
    #define STRUCT_PACKED_END __attribute__((aligned(1), packed))
    #endif

    typedef struct STRUCT_PACKED_START
    {
    UINT32 AddressLength; /**< \brief Address and Length*/
    #define SM_ADDRESS_MASK 0x0000FFFF /**< \brief Address mask*/
    #define SM_LENGTH_MASK 0xFFFF0000 /**< \brief Length mask*/
    #define SM_LENGTH_SHIFT 16 /**< \brief Length shift*/

    UINT32 Settings[1]; /**< \brief Register values 0x0804 : 0x0807*/

    /*Defines to access :
    * - SM Control register 0x0804
    * - SM Status register 0x0805
    * - SM Active register 0x0806
    * - SM PDI Control register 0x0807
    *
    * all defines are based on 0x0804
    */

    /*SyncManger control (0x0804) access*/
    #define SM_SETTING_CONTROL_OFFSET 0 /**< \brief Offset to value of register 0x0804*/
    #define SM_SETTING_ACTIVATE_OFFSET 0 /**< \brief Offset to value of register 0x0806*/
    #define SM_SETTING_CONTROL_MASK 0x0000FFFF /**< \brief Mask to get all SyncManager control values*/
    #define SM_SETTING_MODE_MASK 0x00000002 /**< \brief SyncManager mode mask*/
    #define SM_SETTING_MODE_THREE_BUFFER_VALUE 0x00000000 /**< \brief SyncManager 3Buffer mode value*/
    #define SM_SETTING_MODE_ONE_BUFFER_VALUE 0x00000002 /**< \brief SyncManager 1Buffer mode value*/
    #define SM_SETTING_DIRECTION_MASK 0x0000000C /**< \brief SyncManager direction mask*/
    #define SM_SETTING_DIRECTION_READ_VALUE 0x00000000 /**< \brief SyncManager read direction*/
    #define SM_SETTING_DIRECTION_WRITE_VALUE 0x00000004 /**< \brief SyncManager write direction*/
    #define SM_SETTING_WATCHDOG_VALUE 0x00000040 /**< \brief SyncManager watchdog value*/
    /*SyncManger status (0x0805) access*/
    #define SM_STATUS_MBX_BUFFER_FULL 0x00000800 /**< \brief Indicates in one buffer mode if buffer was completely written*/

    /*SyncManger activate (0x0806) access*/
    #define SM_SETTING_ENABLE_VALUE 0x00010000 /**< \brief SyncManager enable value*/
    #define SM_SETTING_ENABLE_SHIFT 16 /**< \brief SyncManager enable shift*/
    #define SM_SETTING_REPAET_REQ_MASK 0x00020000 /**< \brief SyncManager repeat request mask*/
    #define SM_SETTING_REPEAT_REQ_SHIFT 16 /**< \brief SyncManager repeat request shift*/

    /*SyncManger PDI Control (0x0807) access*/
    #define SM_SETTING_PDI_DISABLE 0x01000000 /**< \brief Bit0 of register 0x0807 (if 1 SM is disabled from PDI)*/
    #define SM_SETTING_REPEAT_ACK 0x02000000 /**< \brief Bit1 of register 0x0807*/

    }STRUCT_PACKED_END
    TSYNCMAN;

    编译器版本:C2800 Compiler Tools 6.4.2 

                           C/C++ GCC Cross Compiler Support  8.5.0.201409172108

  • 具体哪一行是176行呢?要将报错信息与相应的代码对应起来呀。

  • }STRUCT_PACKED_END  <---- 176行

  • OK, C2000不支持单字节对齐,请参考这个帖子最后两个回复:

    http://www.deyisupport.com/question_answer/microcontrollers/c2000/f/56/t/108961.aspx

  • 兄弟,解决没有?我也遇到同样的问题。

  • 同遇到这问题,题主可以说下解决方案吗? 您的帮助是我们学习前进的巨大动力啊,哈哈