This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位專家好,
我是使用28069進行專案的開發
今日在修改cmd檔時不小心將.cinit段的位置修改到
此後使用JTAG進行燒入時,都會出現
C28xx: Error connecting to the target: (Error -1155 @ 0x0) Device may be operating in low-power mode. The debugger has forced the device to wake up. Choose 'OK' to attempt to complete the debug connection. (Emulation package 6.0.228.0)
已確認供電電壓正常,並且通過 "Test Connection"是成功的
請教各位要如何解決這個問題?
t通过目标配置里面启动相应配置文件,然后选择连接目标,连上目标板后,在tools里面选择on chip flash,然后把芯片解锁后擦除芯片程序试一下。