This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335采样问题,望大家能不吝赐教



因为DSP控制板采样有问题,所以进行一步一步调试。给DSP正常供电后,直接给其模拟输入口和模拟地(模拟地与ADCLO相连)之间输入0-3V电压信号,可以正常采样,采样精度尚可。这证明非软件问题和供电问题。然而将此模拟输入电压经过一个运放跟随和RC滤波后再输入给AD口(这是因为完整控制板中,信号会经过一系列调理滤波再输入AD口的),此时采样就出问题了。问题表现在采样数值完全不对,而且最高数值为2000多一点,不到2100,而不是4095。测量过运放跟随和RC滤波后的电压信号,很正常,这说明非运放硬件问题。自己想了半天也不知道什么问题,希望大家能帮助我 。另外请问28335的AD模拟输入口有输入电流大小的要求吗?