TMS320F28P551SG-FS: fast 相关参数

Part Number: TMS320F28P551SG-FS

C:\Users\TI_FUZAI\universal_motorcontrol_lab_f280013x  你好,我使用的是官方例程,自己开发的板子,电机极对数20,最高转速频率1333hz,当前发现,,相电压截止频率388hz

#define USER_M1_EST_FLUX_HF_SF             0.12// (0.10)

//! \brief Defines the scale factor for the frequency estimation
//! the default value is 1.0f, change the value between 0.5f and 1.5f
//!
#define USER_M1_EST_FREQ_HF_SF               1 // 0.70// (0.52)

//! \brief Defines the scale factor for the bemf estimation
//! the default value is 1.0f, change the value between 0.50f and 1.25f
//!
#define USER_M1_EST_BEMF_HF_SF             1//0.80// (0.52f)  这三个参数会影响最高转速的稳定性与效率,尤其USER_M1_EST_BEMF_HF_SF    必须要小,都改到0.42了,否则高转速效率变低, USER_M1_EST_FLUX_HF_SF              这个改成0.3 空在就会异响,
 
  1,问这三个参数该怎么调,
2,    其次  相电压截止频率硬件软件同时改为1700HZ ,三个参数可以同时为1,空载都正常,但是带负载还存在高转速效率低问题,  USER_M1_EST_BEMF_HF_SF     这个值越高越效率越低,感觉影响了角度,
3,当前相电压截止频率 多少合适,希望能给出具体的文档介绍,