This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377SPTP的下载程序问题



之前我们申请过10片TMX320F28377SPTP,并用此开发了一套电源的控制板,开发环境是6.0.1.00040;我们另外买了TMS320F28377SPTP用在同一版本的控制板上,先加载F28377S.ccxml,然后连接目标CPU,在Debug的环境下,选择RUN菜单中Load子菜单中的Load Program,选择相应的Out文件后点“OK”。

先加载F28377S.ccxml,

 

 

 

 

然后连接目标CPU,

连接后:

 

在Debug的环境下,选择RUN菜单中Load子菜单中的Load Program,选择相应的Out文件后点“OK”。

 

C28xx_CPU1: GEL Output:

Memory Map Initialization Complete

C28xx_CPU1: Loader: One or more sections of your program falls into a memory region that is not writable.  These regions will not actually be written to the target.  Check your linker configuration and/or memory map.

C28xx_CPU1: File Loader: Data verification failed at address 0x00080000 Please verify target memory and memory map.

C28xx_CPU1: GEL: File: D:\CCS6WP\zhongshan20160608\CPU1_FLASH\zhongshan20160608.out: a data verification error occurred, file load failed.

请问如何解决?

下载程序时的问题.doc
  • 错误提示你的地址映射错误,检查一下你的CMD文件加载是否正确。

  • 谢谢。我是直接用TI提供的,并且是直接添加到工程中。


    MEMORY
    {
    PAGE 0 : /* Program Memory */
    /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
    /* BEGIN is used for the "boot to Flash" bootloader mode */

    BEGIN : origin = 0x080000, length = 0x000002
    RAMM0 : origin = 0x000122, length = 0x0002DE
    RAMD0 : origin = 0x00B000, length = 0x000800
    RAMLS0 : origin = 0x008000, length = 0x000800
    RAMLS1 : origin = 0x008800, length = 0x000800
    RAMLS2 : origin = 0x009000, length = 0x000800
    RAMLS3 : origin = 0x009800, length = 0x000800
    RAMLS4 : origin = 0x00A000, length = 0x000800
    RESET : origin = 0x3FFFC0, length = 0x000002

    /* Flash sectors */
    FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
    FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
    FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
    FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
    FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
    FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
    FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
    FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
    FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
    FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
    FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
    FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
    FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
    FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */

    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

    BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    RAMD1 : origin = 0x00B800, length = 0x000800

    RAMLS5 : origin = 0x00A800, length = 0x000800

    RAMGS0 : origin = 0x00C000, length = 0x001000
    RAMGS1 : origin = 0x00D000, length = 0x001000
    RAMGS2 : origin = 0x00E000, length = 0x001000
    RAMGS3 : origin = 0x00F000, length = 0x001000
    RAMGS4 : origin = 0x010000, length = 0x001000
    RAMGS5 : origin = 0x011000, length = 0x001000
    RAMGS6 : origin = 0x012000, length = 0x001000
    RAMGS7 : origin = 0x013000, length = 0x001000
    RAMGS8 : origin = 0x014000, length = 0x001000
    RAMGS9 : origin = 0x015000, length = 0x001000
    RAMGS10 : origin = 0x016000, length = 0x001000
    RAMGS11 : origin = 0x017000, length = 0x001000

    }


    SECTIONS
    {
    /* Allocate program areas: */
    .cinit : > FLASHB PAGE = 0
    .pinit : > FLASHB, PAGE = 0
    .text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0
    codestart : > BEGIN PAGE = 0
    ramfuncs : LOAD = FLASHD,
    RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    RUN_SIZE(_RamfuncsRunSize),
    RUN_END(_RamfuncsRunEnd),
    PAGE = 0

    /* Allocate uninitalized data sections: */
    .stack : > RAMM1 PAGE = 1
    .ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1
    .esysmem : > RAMLS5 PAGE = 1

    /* Initalized sections go in Flash */
    .econst : >> FLASHF | FLASHG | FLASHH PAGE = 0
    .switch : > FLASHB PAGE = 0

    .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

    /* The following section definitions are for SDFM examples */
    Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
    Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
    Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
    Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
    Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333
    }

    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */