This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

InstaSPIN HVKit外接仿真器链接不上



尊敬的德州仪器技术人员,

我在调试阶段想用外接仿真器(SEED XDS510PLUS)方式链接我的controlcard 28035,但是链接不上,想问下我该如何处理?

按照High Voltage Motor Control and PFC (R1.1) Kit Hardware Reference Guide说明我做了以下操作:

Jumper set on [M3]-J2

Jumper set on [M3]-J5

[M3]-JP1  USB connection

现在当我检测链接时,我的test connection显示

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'seedjca8990isa.dll'.

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is not generated by TI's USCIF driver or utilities.

The USCIF driver and utilities use the range from -2 down to -999

The value is '+134' (0x00000086).
The title is unavailable.
The explanation is unavailable.

[End]

曹玉