This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我使用28069,用SPIA口进行8bit进行主从通讯,28069为主站。发现配置为16BIT其MOSI口有信号输出,但是配置成8BIT其无信号输出,这中间的配置只是修改了SPICCR的低四位为7,请问这是什么问题呢?
嗯,确实有这样的问题。但是我用CHAR定义的变量在定义联合体后,其字节的数据处理为16bit,这个需要怎么破?】
之前我也遇到这样的问题,其实很容解决.你用示波器看看就明白了.
你可以设成16位模式,看看波形,再设成8位模式看看波形.
DSP28系列,SPI接收与发送都是16位的.如果你发数据如:FA,格式应该是0X00FA.
在DSP28069中 使用CLA 设置一个中断50u,在这个中断中做一个数aa的累加1,然后触发一个CLA任务,任务里面做另外一个数bb的累加1,为什么aa累加到几千,bb才累加一次?使用的是IACK软触发CLA任务