This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335的CAN总线发送问题



最近需要用到28335的CAN总线模块,参照手册做了一下实验,同时参考V141的例程,在例程中是没问题,但是我用USB转CAN连接283335的CAN,最后的结果是28335的CAN一直无法发送成功,一直停在这儿,

do
{
ECanaShadow.CANTA.all = ECanaRegs.CANTA.all;
} while(ECanaShadow.CANTA.bit.TA0 == 0 ); 

说明CAN数据一直没发送出去,同时can的波特率设置如下:系统时钟频率为150MHz,则CAN总线的波特率为500k,其它配置就是V141

ECanaShadow.CANBTC.bit.BRPREG = 9;
ECanaShadow.CANBTC.bit.TSEG2REG = 2;
ECanaShadow.CANBTC.bit.TSEG1REG = 10;

在手册中也有如下说明:

手册中说明是:在任何时候在CAN的网络里面必须一个节点和当前发送节点的波特率相同即可,我用的USB转CAN,波特率设置为500k,并且能够和其它的设备通讯,说明USB转CAN是没问题,现在问题不知道出在哪儿?困惑一周了,大家帮我看看