This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教F2812mcbsp用作SPI(主设备)问题

Other Parts Discussed in Thread: ADS1271

请教各位专家、大侠:

        我用F2812mcbsp用作SPI和ADS1271通信,只用到CLKX和DR管脚,但初始化后,在读取数据时,CLKX无时钟产生,一直保持高电平,初始化设置如下:

void InitMcbsp(void)
{
 EALLOW;
 GpioMuxRegs.GPFMUX.bit.MCLKXA_GPIOF8=1;
 GpioMuxRegs.GPFMUX.bit.MDRA_GPIOF13=1; 
 GpioMuxRegs.GPFMUX.bit.MDXA_GPIOF12=1;
 GpioMuxRegs.GPFMUX.bit.MFSXA_GPIOF10=1;
 EDIS;
  
 McbspRegs.SPCR2.bit.XRST = 0;
 McbspRegs.SPCR1.bit.RRST = 0;
  McbspRegs.SPCR2.bit.GRST = 0;
  
  //Mcbsp配置成SPI主设备
  
 McbspRegs.SPCR1.bit.CLKSTP = 1;
 McbspRegs.PCR1.bit.CLKXP = 1;
// McbspRegs.PCR1.bit.CLKRP = 1;
 McbspRegs.PCR1.bit.CLKXM = 1;
 McbspRegs.PCR1.bit.SCLKME = 0;
 McbspRegs.SRGR2.bit.CLKSM= 1;
 McbspRegs.SRGR1.bit.CLKGDV = 0xaa;
 
 McbspRegs.PCR1.bit.FSXM = 1;
 McbspRegs.SRGR2.bit.FSGM = 0;
 McbspRegs.PCR1.bit.FSXP=1;
 McbspRegs.XCR2.bit.XDATDLY = 1;
 McbspRegs.RCR2.bit.RDATDLY = 1;
 
 McbspRegs.SPCR1.bit.DXENA=1;
 
 
 McbspRegs.RCR1.bit.RWDLEN1 = 1;
 McbspRegs.XCR1.bit.XWDLEN1 = 1;
 
 McbspRegs.PCR1.bit.FSRM = 1;
   //使能
 NOP;
 NOP;
 
 McbspRegs.SPCR2.bit.GRST = 1;
 NOP;
 NOP;
  McbspRegs.SPCR2.bit.XRST = 1;
  McbspRegs.SPCR1.bit.RRST = 1;
 NOP;
 NOP;
// PieCtrl.PIEIER6.bit.INTx5 = 1;
// PieCtrl.PIEIER6.bit.INTx6 = 1;
}

在读程序中,我已经写了,先发数据,产生时钟,再读数据, SysCtrlRegs.PCLKCR.bit.MCBSPENCLK =1也已经设置。

请帮忙指教,设置有什么问题?谢谢了!