This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于cpu1和cpu2下载到FLASH的问题



下面的代码 需要在CPU1  和CPU2  都要写吗?  为什么有的样例中比如 blinky的双核样例 只有cpu2中有这段代码,但是RAMmanagement的样例中 cpu1和cpu2 中都有? 

extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadSize;
extern Uint16 RamfuncsRunStart;

memcpy(&isrfuncRunStart, &isrfuncLoadStart, (uint32_t)&isrfuncLoadSize);