This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2837xS “Technical Reference Manual P1578-P1580 AQCTLA和AQCTLA2 影子寄存器

问题:AQCTLA2是否存在影子寄存器?

AQCTLA存在影子寄存器,在AQCTL寄存器中设定了AQCTLA开启影子/立刻模式,以及什么事件让AQCTLA由影子寄存器装载至实际执行的AQCTLA中。

AQCTLA2和AQCTLA其实一样,都是控制A的输出(仅仅事件不同)。但是手册中没有提到任何关于AQCTLA2是否有影子寄存器,如何装载等信息?

另外,P1484页和P1572关于GLDCFG全局装载配置寄存器中提到,AQCTLA2和AQCTLA既可以受到全局装载信号的控制,也可以受到自身装载配置的控制。

所以我怀疑:AQCTLA2的影子和装载和AQCTLA寄存器一样,TI是不是漏写了?????

  • 如下面帖子回复,我认为你的猜想应该是正确的,不过也不能确定,所以我已经将你这个问题转给美国的C2000产品线专门负责EPWM模块的专家,相信他们很快会在E2E上给你满意的答复。

    http://www.deyisupport.com/question_answer/microcontrollers/c2000/f/56/p/114119/311189.aspx#311189

  • 谢谢你的回复,看文档是一件很累人的事。多谢细心和耐心的回复

    如果可以的话,可否给我留个您的邮箱呢。

    我的邮箱maopeng@ncut.edu.cn

  • 您好,我最近也在研究这个问题,但是我用的是28335,AQ子模块没有映射寄存器,正纠结怎么处理

  • 请问关于28335的AQCTL模块立即生效的问题您有没有解决方法,我现在也困在这个问题上了。非常感谢!

  • F28335不支持,它的EPWM模块是type 0版本,而F2837xS已经升级到了type 4,请参考文档说明。

x 出现错误。请重试或与管理员联系。