This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M和BOOSTXL-DRV8305EVM

Other Parts Discussed in Thread: LAUNCHXL-F28069M, BOOSTXL-DRV8305EVM, MOTORWARE, INSTASPINUNIVERSALGUI

你好:

    现在学习InstaSPIN技术,使用的控制板为LAUNCHXL-F28069M,驱动板为BOOSTXL-DRV8305EVM配套使用控制24VBLDC。学习中遇到若干问题,寻求解答。

    1. 手册中有写:

    

    但是我的电脑硬件扫描不到:

    

    请问为什么?

2. 查看手册中接口略有区别,主要是母线电压采集进28069M的通道不同,请问LAUNCHXL-F28069M和BOOSTXL-DRV8305EVM可以配套使用吗?配套使用的话需要做那些软硬件修改?

3. 使用guicomposer对系统进行应用时,发现24V的母线电压采集到的总是16-17V左右,不加母线电压时为13V,请问这是什么情况?所用代码为例程中Lab02C。

  • 1.安装完ccsv5,LAUNCHXL-F28069M仿真器自动安装;

    2.LAUNCHXL-F28069M和BOOSTXL-DRV8305EVM可以配套使用,我就是使用的这个。运行正常。motorware中有对应的历程。

    3.检查硬件是否配置错误。

  • 谢谢您的回复。

    1.我的仿真器连接正常,可以正常仿真程序,我指的是手册中的UART COM口,我的确实没有识别出COM口;

    2.请问您用的是例程中的那个Lab?说下Lab编号,我试过好几个,都不行。

    3.我是LAUNCHXL-F28069M和BOOSTXL-DRV8305EVM配套使用,应用的guicomposer版本是instaspinuniversalgui_v105,配套的是TI官网上的24VDC电机。当DCBus接24V时,guicomposer显示的母线电压总是16、17V多,电机识别灯会变绿,但电机始终不会转。

    如果您使用过LAUNCHXL-F28069M和BOOSTXL-DRV8305EVM,方便留下个联系方式吗?请教请教,非常感谢。

  • 历程是没有问题的,lab02b、lab05a和05b我都试过,可以正常运行。

    我的qq:1184211201

  • 谢谢你的回复。

        下午试了下,发现BOOSTXL-DRV8305EVM插装在LAUNCHXL-F28069M的J5那排插针处,而lab02b中代码在没改动的情况下define了J1,屏了J5,改下就好了。太着急都没有细看代码!现在电机能转了,2000转运转正常,误差±5转,但3000转时电机开始抖,转速误差比较大,最大到±300多,可能是电机木有固定吧,接下来再慢慢研究。转速也是从guicomposer中查看的,明天再接示波器看看实际转速吧,能转了已经很开心了  嘿嘿

       不过手册中说的COM口还是没有识别,原理图中ISO芯片隔离了SCI接口,目前硬件都没有识别到。

       记下你的Q了,玩电机控制我是新人,以后多多交流,非常感谢

  • ccs7行吗?