This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHV1PHINVKIT调试问题



我在使用TMDSHV1PHINVKIT开发板调试时在做INCR_BUILD 3时 用GUI开动时,设备要不并网电流出现瞬间就停止然后提示直流母线过压,要不就先显示进入逆变模式可以看到逆变电流形成,然后工作几秒后就停止,仍然会提示直流母线过压。我直流源使用的是DC380V/2A 。dwVoltageLoopOutConst我设置的是输出恒流源是2A的系数。做220V/50HZ并网。程序中电压环应该是不工作的,为什么还会出现DC母线过电压呢?不是很明白,希望技术人员给解答一下。谢谢!

此外,还有一个问题,之前看一个帖子中说过关于LOAD SYMBOLS的问题,技术人员解释过程是:上电, 打开CCS->connect, load symbols only, 不要load .out文件, 打开disassembly window反汇编窗口, 跟踪PC指针的运行。我想问一下关于跟踪PC指针的运行是如何实现的?我在CCS里没有找到这个功能,麻烦也解答一下吧。谢谢!