This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

希望得到TI工程师回复:关于TI高压电机控制套件TMDSHVMTRINSPIN母线电压检测故障问题

Other Parts Discussed in Thread: TMDSHVMTRINSPIN

新买的TI高压电机控制套件TMDSHVMTRINSPIN,评估TI的InstaSPIN-foc。

三相电机控制套件:350V、10A、1-1.5 kW,带 Piccolo F28069M、InstaSPIN™-FOC 

按照文档中的说明,进行硬件配置:

Controlcard使用套件中的TMDSCNCD28069MISO,使用直流供电(60V)连接仿真器可以正常连接。

直流供电(60V)不加时,运行lab02b,enablesystem = 1,此时的Dcbus = 11V,这是什么原因?

60V加电后,检测vdcbus = 1V,这是什么原因,电机辨识程序状态机可以正常运行,但电机没有转是什么原因?

希望得到TI工程师~非常感谢!