This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI piccolo手册中“对于可以用作ePWM的输出的引脚,默认内部上拉电阻禁止使能“,请问如果ePWM上拉电阻使能的话会有什么后果?谢谢!



void InitEPwm1Gpio(void)
{
   EALLOW;

/* Disable internal pull-up for the selected output pins
   for reduced power consumption */
// Pull-ups can be enabled or disabled by the user.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1;    // Disable pull-up on GPIO0 (EPWM1A)
    GpioCtrlRegs.GPAPUD.bit.GPIO1 = 1;    // Disable pull-up on GPIO1 (EPWM1B)

/* Configure EPWM-1 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be EPWM1 functional pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1;   // Configure GPIO0 as EPWM1A
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1;   // Configure GPIO1 as EPWM1B

    EDIS;
}

改为

void InitEPwm1Gpio(void)
{
   EALLOW;

/* Disable internal pull-up for the selected output pins
   for reduced power consumption */
// Pull-ups can be enabled or disabled by the user.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0   // Enable pull-up on GPIO0 (EPWM1A)
    GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0    // Enalbe pull-up on GPIO1 (EPWM1B)

/* Configure EPWM-1 pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be EPWM1 functional pins.
// Comment out other unwanted lines.

    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1;   // Configure GPIO0 as EPWM1A
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1;   // Configure GPIO1 as EPWM1B

    EDIS;
}

  • void InitEPwm1Gpio(void)
    {
       EALLOW;

    /* Disable internal pull-up for the selected output pins
       for reduced power consumption */
    // Pull-ups can be enabled or disabled by the user.
    // Comment out other unwanted lines.

        GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1;    // Disable pull-up on GPIO0 (EPWM1A)
        GpioCtrlRegs.GPAPUD.bit.GPIO1 = 1;    // Disable pull-up on GPIO1 (EPWM1B)

    /* Configure EPWM-1 pins using GPIO regs*/
    // This specifies which of the possible GPIO pins will be EPWM1 functional pins.
    // Comment out other unwanted lines.

        GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1;   // Configure GPIO0 as EPWM1A
        GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1;   // Configure GPIO1 as EPWM1B

        EDIS;
    }

    改为

    void InitEPwm1Gpio(void)
    {
       EALLOW;

    /* Disable internal pull-up for the selected output pins
       for reduced power consumption */
    // Pull-ups can be enabled or disabled by the user.
    // Comment out other unwanted lines.

        GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0   // Enable pull-up on GPIO0 (EPWM1A)
        GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0    // Enalbe pull-up on GPIO1 (EPWM1B)

    /* Configure EPWM-1 pins using GPIO regs*/
    // This specifies which of the possible GPIO pins will be EPWM1 functional pins.
    // Comment out other unwanted lines.

        GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1;   // Configure GPIO0 as EPWM1A
        GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1;   // Configure GPIO1 as EPWM1B

        EDIS;
    }

    以上标注语句你是要PWM内部上拉使能还是禁止?默认可以复用为PWM的引脚是内部上拉禁止的,这样在PWM GPIO没初始化之前,这几个GPIO是输入高阻态,从管脚上看没有很强的外部干扰,管脚就是低电平,而其他GPIO是默认内部上拉使能的,也就是你下面那部分标注语句的形态。所以在未初始化时,你会看到管脚是高电平。PWM管脚这么设置的原因是防止功率管在初始化时就被打开造成短路,因为大多数的驱动芯片都是不带反向功能的。