This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI工程组合问题

在几个工程合成一个工程时:出现这个警告:creating:“sysmem” section with default size of 0x400:use   这个怎么回事?

  • 你的system的段的位置和大小在CMD中是不是变过?确认下大小够不够

  • cmd文件有改过,这是我的CMD文件。

    MEMORY
    {
    PAGE 0 : /* Program Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    RAML0 : origin = 0x008000, length = 0x000c00 /* on-chip RAM block L0 */
    OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
    FLASHA : origin = 0x3D8000, length = 0x01FF80
    CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

    FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */
    IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
    IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
    IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

    ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
    /* Registers remain on PAGE1 */

    BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
    RAMM0 : origin = 0x000050, length = 0x0007B0 /* on-chip RAM block M0 */
    RAML2 : origin = 0x008C00, length = 0x007400 /* on-chip RAM block L2 */
    USB_RAM : origin = 0x040000, length = 0x000800 /* USB RAM */

    }

    /* Allocate sections to memory blocks.
    Note:
    codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
    execution when booting to flash
    ramfuncs user defined section to store functions that will be copied from Flash into RAM
    */


    SECTIONS
    {

    /* Allocate program areas: */
    .cinit : > FLASHA, PAGE = 0
    .pinit : > FLASHA, PAGE = 0
    .text : > FLASHA, PAGE = 0
    codestart : > BEGIN, PAGE = 0
    ramfuncs : LOAD = FLASHA,
    RUN = RAML0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    PAGE = 0

    csmpasswds : > CSM_PWL_P0, PAGE = 0
    csm_rsvd : > CSM_RSVD, PAGE = 0

    /* Allocate uninitalized data sections: */
    .stack : > RAMM0, PAGE = 1
    .cio : > RAMM0, PAGE = 1
    .sysmem : > RAML2, PAGE = 1
    .ebss : > RAML2, PAGE = 1
    .esysmem : > RAML2, PAGE = 1


    /* Initalized sections to go in Flash */
    /* For SDFlash to program these, they must be allocated to page 0 */
    .econst : > FLASHA, PAGE = 0
    .switch : > FLASHA, PAGE = 0

    /* Allocate IQ math areas: */
    IQmath : > FLASHA, PAGE = 0 /* Math Code */
    IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD

    /* Allocate FPU math areas: */
    FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD

    //DMARAML5 : > RAML5, PAGE = 1
    data1 : > USB_RAM, PAGE = 1
    data2 : > USB_RAM, PAGE = 1
    data3 : > USB_RAM, PAGE = 1
    data4 : > USB_RAM, PAGE = 1

    /* Uncomment the section below if calling the IQNexp() or IQexp()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

    }
    */