AD采样程序如下:
GpioDataRegs.GPASET.bit.GPIO12 = 1; //测试时间
AdcRegs.ADCSOCFRC1.all = 0xFFFF; //软件触发AD采样
while (AdcRegs.ADCINTFLG.bit.ADCINT1 == 0){} //AD采样结束
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Must clear ADCINT1 flag since INT1CONT = 0
GpioDataRegs.GPACLEAR.bit.GPIO12 = 1; //测试时间
AD使用软件触发,SOC15触发INT,观察GPIO12的高低电平测量AD采样时间,但是观察到的高电平时间只有280ns,比一次采样的最小时间(400ns)还短,并且改变采样窗宽度对时间没有影响,这是什么原因?