This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DSP28035用max3232转换232电平通过SCImode烧写程序有问题

Other Parts Discussed in Thread: MAX3232, MAX232

关于DSP28035用max3232转换232电平通过SCImode烧写程序有问题:
首先自己做的板子,一开始以为是max3232电路有问题,后面通过示波器观察发现电路正常工作,也排除了串口线有问题;接着我换了一个外接的max232的模块做测试,结果一样烧写不了程序;然后我用了一个USB转TTL的模块来烧写发现烧写成功,我又开始怀疑我的板子有问题,又拿了我买的开发板测试,结果发现现象跟我的一样:用max3232或max232芯片做的电平转换电路烧写失败,用USB转TTL的USB转串口模块烧写程序成功!

我想知道是不是我哪里做的有问题?还是这款芯片本来就这样?