This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

InstaSPIN-FOC lab 11问题请教

lab11为A Simplified Example without Controller Module,程序中有如下代码:

#ifdef FAST_ROM_V1p6
{
// These function calls are used to initialize the estimator with ROM
// function calls. It needs the specific address where the controller
// object is declared by the ROM code.
CTRL_Handle ctrlHandle = CTRL_init((void *)USER_CTRL_HANDLE_ADDRESS
,0x200);
CTRL_Obj *obj = (CTRL_Obj *)ctrlHandle;

// this sets the estimator handle (part of the controller object) to
// the same value initialized above by the EST_init() function call.
// This is done so the next function implemented in ROM, can
// successfully initialize the estimator as part of the controller
// object.
obj->estHandle = estHandle;

// initialize the estimator through the controller. These three
// function calls are needed for the F2806xF/M implementation of
// InstaSPIN.
CTRL_setParams(ctrlHandle,&gUserParams);
CTRL_setUserMotorParams(ctrlHandle);
CTRL_setupEstIdleState(ctrlHandle);
}
#else
{
// initialize the estimator. These two function calls are needed for
// the F2802xF implementation of InstaSPIN using the estimator handle
// initialized by EST_init(), these two function calls configure the
// estimator, and they set the estimator in a proper state prior to
// spinning a motor.
EST_setEstParams(estHandle,&gUserParams);
EST_setupEstIdleState(estHandle);
}
#endif

// get Idq from estimator to avoid sin and cos, and a Park transform,
// which saves CPU cycles
EST_getIdq_pu(estHandle,&gIdq_pu);

请问:

1、FAST_ROM_V1p6在哪定义的?程序中找了半天都没找到。

2、CTRL_init()和EST_getIdq_pu()两个函数都是在main.h中声明的,这两个函数的原型在哪?