本人在前一版本可以的28335程序上一直过来的程序,现在出现了编译问题
../include/DSP2833x_common/lib/IQmath.lib<IQ24cosPU.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C28FPU32" specified in a previous file or on the command line DSP28335_ACI C/C++ Problem
../include/DSP2833x_common/lib/IQmath.lib<IQ24div.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line DSP28335_ACI C/C++ Problem
程序中有同时使用浮点跟定点,
所以同时引用了fpu.lib跟iqmath.lib
工程配置也打开了fpu浮点模式
这时候编译就出现问题了
(上一版本可用的28335程序也是同时引用,并无报错,只不过没有用Q格式,全是浮点)
但是,如果不引用iqmath.lib的话,只引用fpu.lib就编译通过
但是程序中关于Q格式计算的=都为0