This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377多台电机控制的疑问

我们期望实现六台交流永磁同步电动机的控制。28377常规使用,可以控制四台电机。我有以下疑问,请问得到大家的帮助。

1、论坛里面有说,外扩一个“driver”可以实现只需要DSP发出上桥臂驱动信号,driver自动生成下桥臂信号,以此解决28377的PWM波路数不够的问题。而我之前没有接触过类似器件,能推荐一个这样的driver吗?

2、双核的28377,可以对每个核独立编程吗?还是由编译器自动分配?

3、假设PWM路数足够驱动六台电动机,请问28377能运行六台交流伺服驱动器的程序吗?

  • 4、假设控制频率为6k,依我们现在的经验,28377S运行控制六台电机的控制程序主中断的时间可能不够。依据您的经验,28377S运行控制六台电机的控制程序主中断的时间够用吗?
    5、如果28377s运行不起来六台电机的控制程序,我们考虑使用28377D,由于28377D是双核,据说28377D能对每个核心独立分配运行程序,想请教一下是否可以实现对每个核独立编程吗?还是由编译器自动分配?
    6,如果23877s和d都不能实现上述功能,还有什么解决方案吗?

  • @ !

       按照我的理解,28377S /28377D去控制6台PMSM或BLDC,如果要做伺服控制、PI、PID,或是更高级的sensorless FOC等算法,资源应该是够的,但CPU开销较大,任务调度、协调复杂。

       28377D是DSP + DSP,两个DSP完全对称,两套程序独立运行,两个DSP可通过MSG RAM或Share RAM,通过IPC进行通讯,协调。

       28377D我没用过,但我用过F28M35,它是DSP + M3,也是两套程序独立运行,双核之间的通讯机制与28377D是一样一样的,我用它设计的产品已量产。

       F28M35是为三轴机器人而生的,按照用你上面说的用drive的方式,到是可以控制6个motor。drive很多,其实就是MOS管驱动器,我用过FairChild: FAN3217TMX;Microchip:TC4428EOA713;IR:IR4428S。你选那种一路高有效,一路低有效的芯片,用一个PWM信号同时接这两个输入信号,两路输出信号一个驱动上桥臂,一个驱动下桥臂,高电平时驱动上桥臂导通,低电平时驱动下桥臂导通,但这样也很麻烦,不太好控制。

  • @ !@anfu lee 

       我也想选用一款芯片控制3个带传感器直流无刷电机,也是用mos管驱动的。

       我想请教一下:一个直流无数电机需要6路Pwm信号输出去控制mos管,同时需要3路Cap来捕获位置信号(比如说霍尔传感器反馈信号)来判断换相,如果我是要控制3个BLDC电机的话,理论上是不是DSP最少要能有18路pwm 和9路的cap?  但是我看你们说的28337和F28M3好像都没有9路的CAP啊,也没有9路的QEP?z这个怎么理解啊?