This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教F28M35寄存器读取等几个问题

想用F28M35做一个小项目,咨询几个问题:

1、M35里的C28核能否直接读取M3核中的寄存器?比如TImer,我想知道能否C28直接读取M3的时钟,还是M3先写到RAM里再由C28读取?这应该是关于MTOC方面的内容,我看了下datasheet,双核间只能通过RAM传递信息?能否互相直接读取寄存器?(延时小)

2、M35是是否支持精密时钟同步,精度多少?想实现时钟同步的话,选的PHY芯片是否可以选一个不支持精密时钟协议的芯片?如果对精度有更高要求,选一个支持更高精度的PHY芯片是否可以达到更高精度。

3、在《不打折扣的性能:利用双子系统微控制器实施实时控制和通信》的文档第三页提到“此外还提供了一种时间戳方法,用于在必要情况下实现同步”,这说的是M3核与C28核之间也能通过时间戳方法实现时钟同步吗? 文档链接: www.ti.com/.../zhcy042