This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000-S320F28027 Piccolo Entry Line Control Pad 例程无法编译

硬件平台使用S320F28027 Piccolo Entry Line Control Pad,在CCS6.2 IDE中使用“Example_F2802x0controlPadDemo”例程:

编译时失败:

错误信息:

Buildfile generation error occurred..
Product 'XDAIS' v0.0 is not currently installed and no compatible version is available. Please install this product or a compatible version.
Build stopped..

请问这个问题如何解决,是因为使用了高版本的CCS么,如果是,哪个版本是合适的呢?

谢谢大家。