This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

批量生产过程中,有部分单板DSP28031莫名其妙原因连不上仿真器

   1、硬件电路介绍:DSP28031  外接10Mhz的有源晶振  复位芯片用的是SP809EK,仿真器用的是TI原版的XDS100V2仿真器

    2、软件:CCS3.3 (已确定正常)

    问题描述:在批量生产1000片中大约有十多片单板因为在用仿真器烧录Bootloader程序的时候连接不上仿真器。作了如下检查:

    1、检查电源供电正常,用仿真器的电源给DSP供电,DSP有3.3V电压

     2、检查外接晶振起振,频率为10MHZ

     3、检查复位电路正常, 有复位信号

     4、检查JTAG引脚的TCK引脚在连接仿真器的时候会给一段脉冲信号(正常情况下脉冲信号持续几秒钟就消失,此时DSP就连接上仿真器),但是发现脉冲信号一直存在,并且CCS3.3处于Connecting状态,处于死机中,只能关闭仿真器电源结束连接。

     原因分析:

    1、首先排除了软件问题,因为有正常的板子可以连接上

     2、硬件问题可以基本排除复位电路和晶振问题

     3、怀疑DSP芯片坏掉了,但是如果DSP坏掉了,为什么GPIO口还会有高电平输出,并且晶振还起振了

     4、其他电路有故障,但是不能定位到问题原因

     请教各位不知道有何经验或者建议可以分享。