This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28034使用ECAP和EQEP模块测速问题

本人想改善原本的MT法测速问题,原程序中是对AB正交脉冲进行计数,每4个脉冲进行一次计时,比如 1 2 3 4脉冲测速一次, 5  6 7 8脉冲测速一次,通过这个进行测速,但是低速时效果不好。采用ecap模块可以实现最新的四个脉冲测速,形成流水线的形式,每次更新一个。比如 1 2 3 4脉冲测速, 2 3 4 5测速,3 4 5 6测速。每到来一个脉冲可以利用前一刻的,实现延迟最小。但是本人在写程序的时候发现一个问题,程序中如何实现最新的四个脉冲时间计数,因为ecap不采用中断访问的话,absolute time-stamp的时间是存在CAP1-CAP4中,比如前4个的时间 CAP3-CAP1,CAP4-CAP2,CAP1-CAP3,CAP2-CAP4不断循环,可是这个是不断变化的?程序中怎么实现最新的四个脉冲时间保存?(说的有点乱,见谅)