DSP2812的外部中断,我用一个14K和60Hz频率的方波来触发外部中断XINT1 XINT2,然后利用I/O口输出高低电平(方波)。 当用14K来触发时,运行结果正常,产生了一个7K的方波,但是当使用60Hz频率的方波来触发时,结果产生了一个频率从几百到几K波形,后面检查发现两个中断口不管使用XINT1 XINT2 都是14K正常 60Hz不正常 后面发现当输入口悬空时也会产生中断信号!!!1纠结了一天了 不知道什么原因
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DSP2812的外部中断,我用一个14K和60Hz频率的方波来触发外部中断XINT1 XINT2,然后利用I/O口输出高低电平(方波)。 当用14K来触发时,运行结果正常,产生了一个7K的方波,但是当使用60Hz频率的方波来触发时,结果产生了一个频率从几百到几K波形,后面检查发现两个中断口不管使用XINT1 XINT2 都是14K正常 60Hz不正常 后面发现当输入口悬空时也会产生中断信号!!!1纠结了一天了 不知道什么原因
谢谢