This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377D BOOTCTRL 地址的问题

Other Parts Discussed in Thread: CONTROLSUITE

2877D Z1-BOOTCTRL和Z2-BOOTCTRL地址在手册里写的是0x7801E和0x7821E

controlsuite里自带的CMD,2837xD_dcsm_lnk_cpu1.cmd中,地址为0x7801C和0x7821C


/* this linker command file is to be included if user wants to use the DCSM feature on the device
* DCSM means Dual Zone Code Security Module.
* This linker command file works as an addendum ot the already existing Flash/RAM linker command file
* that the project has.
* The sections in the *_ZoneSelectBlock.asm source file is linked as per the commands given in the file
* NOTE - please note fill=0xFFFF, this helps if users include this file in the project by mistake and
* doesn't provide the needed proper *_ZoneSelectBlock.asm sources .
* Please refer to the Blinky DCSM example in the controlsuite examples for proper usage of this.
*
* Once users are confident that they want to program the passwords in OTP, the DSECT section type can be removed.
*
*/

MEMORY
{
PAGE 0 : /* Program Memory */

/* Z1 OTP. LinkPointers */
DCSM_OTP_Z1_LINKPOINTER : origin = 0x78000, length = 0x00000C
/* Z1 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z1_PSWDLOCK : origin = 0x78010, length = 0x000004
/* Z1 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z1_CRCLOCK : origin = 0x78014, length = 0x000004
/* Z1 OTP. RESERVED/BOOTCTRL */
DCSM_OTP_Z1_BOOTCTRL : origin = 0x7801C, length = 0x000004

/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z1 OTP. Z1 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z1_P0 : origin = 0x78020, length = 0x000010

/* Z2 OTP. LinkPointers */
DCSM_OTP_Z2_LINKPOINTER : origin = 0x78200, length = 0x00000C
/* Z2 OTP. GPREG1/GPREG2 */
DCSM_OTP_Z2_GPREG : origin = 0x7820C, length = 0x000004
/* Z2 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z2_PSWDLOCK : origin = 0x78210, length = 0x000004
/* Z2 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z2_CRCLOCK : origin = 0x78214, length = 0x000004
/* Z2 OTP. GPREG3/BOOTCTRL */
DCSM_OTP_Z2_BOOTCTRL : origin = 0x7821C, length = 0x000004

/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z2 OTP. Z2 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z2_P0 : origin = 0x78220, length = 0x000010

}

SECTIONS
{
dcsm_otp_z1_linkpointer : > DCSM_OTP_Z1_LINKPOINTER PAGE = 0, type = DSECT
dcsm_otp_z1_pswdlock : > DCSM_OTP_Z1_PSWDLOCK PAGE = 0, type = DSECT
dcsm_otp_z1_crclock : > DCSM_OTP_Z1_CRCLOCK PAGE = 0, type = DSECT
dcsm_otp_z1_bootctrl : > DCSM_OTP_Z1_BOOTCTRL PAGE = 0, type = DSECT
dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P0 PAGE = 0, type = DSECT

dcsm_otp_z2_linkpointer : > DCSM_OTP_Z2_LINKPOINTER PAGE = 0, type = DSECT
dcsm_otp_z2_pswdlock : > DCSM_OTP_Z2_PSWDLOCK PAGE = 0, type = DSECT
dcsm_otp_z2_crclock : > DCSM_OTP_Z2_CRCLOCK PAGE = 0, type = DSECT
dcsm_otp_z2_bootctrl : > DCSM_OTP_Z2_BOOTCTRL PAGE = 0, type = DSECT
dcsm_zsel_z2 : > DCSM_ZSEL_Z2_P0 PAGE = 0, type = DSECT
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

应该以哪个为准