PWM1和PWM2被设置成同步,单步运行时EPwmxRegs.TBCTR里的值也是一样的,但是连续运行时,发现watch windows 里面的EPwm1Regs.TBCTR和EPwm4Regs.TBCTR的值是不一样的,但是停止运行程序后,EPwm1Regs.TBCTR和EPwm4Regs.TBCTR的值又都变成一样的了,
请问这是怎么回事?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PWM1和PWM2被设置成同步,单步运行时EPwmxRegs.TBCTR里的值也是一样的,但是连续运行时,发现watch windows 里面的EPwm1Regs.TBCTR和EPwm4Regs.TBCTR的值是不一样的,但是停止运行程序后,EPwm1Regs.TBCTR和EPwm4Regs.TBCTR的值又都变成一样的了,
请问这是怎么回事?谢谢!
你好,你说的“epwm_timer_interrupts例程”,是全局时钟同步,
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through
EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through
EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through
EPwm5Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through
EPwm6Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through
EPwmx.Regs.TBCTL.bit.SYNCOSEL 设置成0 ,1,2都没有关系吧?
本想这个问题到此为止的,但是想想离想要的结果还有一步就再问下吧,叨扰了,先谢谢了!
设置如图:
2. 然后,右键选取仿真配置里的“lanch selected configuration”
3.连接上仿真器和控制板,加载编译好的程序,选择实时查看和刷新 ,再点击连续运行
发现他们的值还是不一样,但是停止运行程序后,所有的结果又变成一样了。
我的软件是CCSV5,前几天才全部更新了一遍。
请指正错误,谢谢!
没有把我的配置 335USB2.ccxml设置成默认。在默认的情况下,右键其属性,选择上halt target的属性,再lauch 连接,实时模式下刷新,连续运行就可以了。