This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS6.0中Run in RAM 和Run in Flash 选择 在哪里设置



请问 CCS6.0中Run in RAM 和Run in Flash  选择 在哪里设置?

CCS4 中是这么设置的:

 Set the build configuration by clicking the menu: Project\Active Build Configuration. If
user want to run the code the in RAM, please choose the RAM option, or the FLASH
option need to be chose.

但是在CCS6中 的project 下 找不到Active build Configuration