This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI原厂Spectrum Digital仿真器XDS560v2STM突然无法与目标板连接



调试28335时发生的问题,2周没有连接目标板,今天连接调试突然发现仿真器与DSP连不上了,工程什么都没有动,点击test connection出现如下提示:

是不是仿真器烧毁了啊,1万多的仿真器啊,要挨骂了

[Start: Spectrum Digital XDS560V2 STM USB Emulator_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\Administrator\AppData\Local\Texas Instruments\
CCS\ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_conf
Download failed for file C:\ti\ccsv6\ccs_base\common\uscif\xds560v2.out

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.

[End: Spectrum Digital XDS560V2 STM USB Emulator_0]