This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
section的告警如下:
warning #16002-D: build attribute vendor section TI missing in "../lib/IQmath.lib<IQ24div.obj>": compatibility cannot be determined
warning #16002-D: build attribute vendor section TI missing in "../lib/IQmath.lib<IQmathTables.obj>": compatibility cannot be determined
但这应该不是原因。
CMD文件配置如下:
/*==================================================================================*/
/* User specific Linker command file for running from FLASH */
/*==================================================================================*/
/* FILE: F28035_FLASH_HVBLDC_Sensored.CMD */
/* */
/* Description: Linker command file for User custom sections targetted to run */
/* from FLASH. */
/* */
/* Target: TMS320F28035 */
/* */
/* Version: 1.00 */
/* */
/*----------------------------------------------------------------------------------*/
/* Copyright Texas Instruments 锟�009 */
/*----------------------------------------------------------------------------------*/
/* Revision History: */
/*----------------------------------------------------------------------------------*/
/* Date | Description */
/*----------------------------------------------------------------------------------*/
/* 4/13/09 | Release 1.0 New release. */
/*----------------------------------------------------------------------------------*/
/* Define the memory block start/length for the F28035
PAGE 0 will be used to organize program sections
PAGE 1 will be used to organize data sections
Notes:
Memory blocks on F2803x are uniform (ie same
physical memory) in both PAGE 0 and PAGE 1.
That is the same memory region should not be
defined for both PAGE 0 and PAGE 1.
Doing so will result in corruption of program
and/or data.
L0 memory block is mirrored - that is
it can be accessed in high memory or low memory.
For simplicity only one instance is used in this
linker file.
Contiguous SARAM memory blocks or flash sectors can be
be combined if required to create a larger memory block.
*/
MEMORY
{
/* Note that the memory allocation below does not create sections as necessary for
the CLA on the F2803x.
*/
PAGE 0:
progRAM : origin = 0x008000, length = 0x001000 /* on-chip RAM (L0-L2)*/
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */
FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */
FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */
FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */
FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */
FLASHC : origin = 0x3F2000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
BOOTROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 :
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
dataRAM : origin = 0x009000, length = 0x001000 /* data RAM (L3) */
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
CLA_CPU_MSGRAM : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */
CPU_CLA_MSGRAM : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA, PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHC, PAGE = 0//FLASHA to FLASHC
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = progRAM,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0, PAGE = 1
.ebss : > dataRAM, PAGE = 1
.esysmem : > dataRAM, PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
Cla1ToCpuMsgRAM : > CLA_CPU_MSGRAM PAGE = 1
CpuToCla1MsgRAM : > CPU_CLA_MSGRAM PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
}
*/
}
SECTIONS
{
Net_terminals: > dataRAM,PAGE = 1
DLOG:> dataRAM,PAGE=1
}
C2Prog的用户手册(菜单Help -> Manual)里说得非常清楚,需要使用以下命令进行.out文件到.hex格式的转换(2.2 Hex File Generation):
c2000-tools:
hex2000 -romwidth 16 -memwidth 16 -i -o .\Debug\test.hex .\Debug\test.out
为什么在上面最后两个截图的配置里既不使用post-build进行.out文件的后端处理,还使用-intel生成了intel格式呢?
.
你可以将生成的.out文件copy到编译器安装路径下,通过dos command line按照以上命令进行转换。
也可以通过下面的编译选项先默认选择Intel-hex,然后在上方的post-build编辑框里修改其命令格式满足C2Prog要求的格式进行编译,并直接转换,这样在debug文件夹下会同时生成.out文件和可用于C2Prog烧录的.hex文件。
PS:印象里不修改也可以直接使用,你可以对比试试。我没有试过。:)
那建议你使用第一种方法吧。
你的编译器可能不支持这个选项,可以在以下链接里下载比较新的版本,然后添加进来到CCS IDE里:
http://software-dl.ti.com/codegen/non-esd/downloads/download.htm#C2000
之后在工程里选择更高版本的就会有这个显示了。
您好 我已经在您提供的链接中下载了一个ti_cgt_c2000_17.6.0.STS_windows_installer。已经安装好了 请问如何添加到CCS IDE里。我用的ccs版本是 Version: 6.1.3.00033