This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

drv8301 revd硬件电路疑问



在void HAL_cal(HAL_Handle handle)有使用IC_FB进行HAL_AdcOffsetSelfCal(handle),IB_FB进行HAL_OscTempComp(handle)校准,直接去掉硬件接口IC_FB、IC_FB,真的没有影响吗?

void HAL_cal(HAL_Handle handle)
{
  HAL_Obj *obj = (HAL_Obj *)handle;


  // enable the ADC clock
  CLK_enableAdcClock(obj->clkHandle);


  // Run the Device_cal() function
  // This function copies the ADC and oscillator calibration values from TI reserved
  // OTP into the appropriate trim registers
  // This boot ROM automatically calls this function to calibrate the interal
  // oscillators and ADC with device specific calibration data.
  // If the boot ROM is bypassed by Code Composer Studio during the development process,
  // then the calibration must be initialized by the application
  ENABLE_PROTECTED_REGISTER_WRITE_MODE;
  (*Device_cal)();
  DISABLE_PROTECTED_REGISTER_WRITE_MODE;

  // run offsets calibration in user's memory
  HAL_AdcOffsetSelfCal(handle);

  // run oscillator compensation
  HAL_OscTempComp(handle);

  // disable the ADC clock
  CLK_disableAdcClock(obj->clkHandle);

  return;
} // end of HAL_cal() function

 

// set SOC0 channel select to ADCINA5
  ADC_setSocChanNumber(obj->adcHandle, ADC_SocNumber_0, ADC_SocChanNumber_A5);

 

 //Select channel B5 for all SOC
  HAL_AdcCalChanSelect(handle, ADC_SocChanNumber_B5);