This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何实现28027的GPIO引脚复位后一直是高电平?手册里没有介绍内部上拉电阻配置,通用GPIO貌似没有上拉电阻。



我将28027芯片  GPIO0 GPIO1 配置为IO输出模式,用过main程序里将GPIO0默认拉高备用,但是通过示波器观察发现复位后一小段时间是低电平。查阅28027手册,没发现有介绍说有内部上拉或下拉电阻。上电复位默认低电平这种有没有什么办法可以改为上电复位是高电平? 软件配置有没有这个选项?  如果软件只是设置为常规输出型GPIO,可否通过外部加上拉电阻的方法来实现默认输出高电平的目的?谢谢。