专家您好:
我用的是F2801,在IO复用成PWM波功能的情况下,配置对称模式,通过CAU =1,以及CAD=2产生占空比。若此时令CMP=0使占空比=0,我想请教下,此时IO口输出就是一直是低电平吗?有没有一个很窄的示波器都不能分辨的脉冲呢?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
专家您好:
我用的是F2801,在IO复用成PWM波功能的情况下,配置对称模式,通过CAU =1,以及CAD=2产生占空比。若此时令CMP=0使占空比=0,我想请教下,此时IO口输出就是一直是低电平吗?有没有一个很窄的示波器都不能分辨的脉冲呢?
谢谢!
“此时”是Counter走到哪里的什么时候呢? 如果楼主想产生一个0%~100%的PWM波形,可以参考附件中的文档。