This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28035的CLA触发问题



请问若用AD中断触发CLA后,AD中断程序和CLA task中的程序处理是并行的吗?如果中断程序处理完成而CLA task还在执行,会不会有什么影响?

  • 我想你可能还没有完全理解CLA是做什么的。

    当使用ADC中断触发CLA执行任务后,CLA里面的任务就可以处理之前在C28x里的ADC中断里的所有事情,也就是说,这时完全没有必要再触发ADC中断在C28x里运行。你自己需要决定,到底是由C28x来执行ADC中断,还是CLA来执行。当然也可以同时使能,但通常来说,不会这样做。即便同时执行,它们的程序也是独立运行的,除非你自己有让它们之间交换数据,或实施同一外设的寄存器控制,那么它们不会互相影响。