This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M36P63C2 程序下载问题

使用 F28M36P63C2 作为主控,但是在调试F28M36P63C2时,遇到了两个问题。

1、串口下载程序问题: 使用TI的UNIFLASH软件通过串口给芯片烧写程序时,提示串口没有连接或不支持该芯片(串口通信测试是正常的)

2、LIB封装使用问题: 将TI提供的底层驱动示例文件先进行LIB封装,然后包含进项目文件进行编译,DEBUG在线调试没问题,但是使能M3引导C28启动时,M3核心可以正常运行,C28核心无法正常启动,可能是没有引导成功还是其他问题。将底层驱动与项目文件一起进行编译,M3核和C28核都没有问题(程序是一样的)

请各位先进帮忙给下意见,谢谢。