自己做了块2812板子,测试时板子和电脑一直连接不上。(1)挨个测试dsp各引脚电源,3.3v和1.8v和GND都正常,其中3.3v和1.8v纹波都不超过+-50mv。
(2)发现dsp上JTAG口的TDO输出一直为1.8v,而正常的dsp为0v!! 想知道是什么原因造成的,而TMS,TCLK这些都为3.3v(不连仿真器)。
(3)CLKOUT输出为3.7MHz的正弦波。
测了好久了,请各位高手指导下,非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
自己做了块2812板子,测试时板子和电脑一直连接不上。(1)挨个测试dsp各引脚电源,3.3v和1.8v和GND都正常,其中3.3v和1.8v纹波都不超过+-50mv。
(2)发现dsp上JTAG口的TDO输出一直为1.8v,而正常的dsp为0v!! 想知道是什么原因造成的,而TMS,TCLK这些都为3.3v(不连仿真器)。
(3)CLKOUT输出为3.7MHz的正弦波。
测了好久了,请各位高手指导下,非常感谢!
Error connecting to the target:
(Error -230 @ 0x0)
The measured lengths of the JTAG IR and DR scan-paths are invalid.
This indicates that an error exists in the link-delay or scan-path.
(Emulation package 5.1.73.0)
连接仿真器,在ccs上connect时 TDO引脚输出信号幅值为3.3v的方波信号