This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI INSTASPIN 下桥臂电阻采样改为U V W电流传感器采样,软件上要改什么地方啊?或者怎样换算符合算法要求?

Other Parts Discussed in Thread: TIDA-00913

TI INSTASPIN 下桥臂电阻采样改为U V W电流传感器采样,软件上要改什么地方啊?或者怎样换算符合算法要求?

  • 首先你要计算一下换算比例,然后修改user.h中的USER_ADC_FULL_SCALE_CURRENT_A

    其次: 修改hal.h中的readAdcData函数,如下标黄色三个值的正负符号,注意,算法里面以流进去电机电流的方向为正,如果你用霍尔采样,再经过运放,最终确定一下这个电流方向,如果反相了,则在value前面加符号。

    static inline void HAL_readAdcData(HAL_Handle handle,HAL_AdcData_t *pAdcData)
    {
    HAL_Obj *obj = (HAL_Obj *)handle;

    _iq value;
    _iq current_sf = HAL_getCurrentScaleFactor(handle);
    _iq voltage_sf = HAL_getVoltageScaleFactor(handle);


    // convert current A
    // sample the first sample twice due to errata sprz342f, ignore the first sample
    value = (_iq)ADC_readResult(obj->adcHandle,ADC_ResultNumber_1);
    value = _IQ12mpy(value,current_sf) - obj->adcBias.I.value[0]; // divide by 2^numAdcBits = 2^12
    pAdcData->I.value[0] = value;

    // convert current B
    value = (_iq)ADC_readResult(obj->adcHandle,ADC_ResultNumber_2);
    value = _IQ12mpy(value,current_sf) - obj->adcBias.I.value[1]; // divide by 2^numAdcBits = 2^12
    pAdcData->I.value[1] = value;

    // convert current C
    value = (_iq)ADC_readResult(obj->adcHandle,ADC_ResultNumber_3);
    value = _IQ12mpy(value,current_sf) - obj->adcBias.I.value[2]; // divide by 2^numAdcBits = 2^12
    pAdcData->I.value[2] = value;

    另外一个函数,updateAdcBias, 如果是正相采样,则bias +=, 否则 -=。

    static inline void HAL_updateAdcBias(HAL_Handle handle)
    {
    uint_least8_t cnt;
    HAL_Obj *obj = (HAL_Obj *)handle;
    _iq bias;


    // update the current bias
    for(cnt=0;cnt<HAL_getNumCurrentSensors(handle);cnt++)
    {
    bias = HAL_getBias(handle,HAL_SensorType_Current,cnt);

    bias += OFFSET_getOffset(obj->offsetHandle_I[cnt]);

    HAL_setBias(handle,HAL_SensorType_Current,cnt,bias);
    }

    ERIC


  • Hi,Eric
    TIDA-00913中提到中断中将PWM取反具体怎么理解?
    interrupt void mainISR(void)
    {
    HAL_PwmData_t negPwmData = {_IQ(0.0), _IQ(0.0), _IQ(0.0)};

    // toggle status LED
    if(gLEDcnt++ > (uint_least32_t)(USER_ISR_FREQ_Hz / LED_BLINK_FREQ_Hz))
    {
    HAL_toggleLed(halHandle,(GPIO_Number_e)HAL_Gpio_LED2);
    gLEDcnt = 0;
    }


    // acknowledge the ADC interrupt
    HAL_acqAdcInt(halHandle,ADC_IntNumber_1);


    // convert the ADC data
    HAL_readAdcData(halHandle,&gAdcData);


    // run the controller
    CTRL_run(ctrlHandle,halHandle,&gAdcData,&negPwmData);
    //每次中断negPwmData初始化为零,那么写入控制运行已经不能运行了吧?


    // negate PwmData generated by SVGEN module in ROM
    gPwmData.Tabc.value[0] = _IQmpy(negPwmData.Tabc.value[0], _IQ(-1.0));
    gPwmData.Tabc.value[1] = _IQmpy(negPwmData.Tabc.value[1], _IQ(-1.0));
    gPwmData.Tabc.value[2] = _IQmpy(negPwmData.Tabc.value[2], _IQ(-1.0));


    // write the PWM compare values
    HAL_writePwmData(halHandle,&gPwmData);


    // setup the controller
    CTRL_setup(ctrlHandle);


    return;
    } // end of mainISR() function